Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contate um especialista

M9391A PXIe Vector Signal Analyzer Instrument Drivers

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

Data de lançamento Versão Descrição da Versão
2017-03-09 2.1.240.2 New FPGA bits for M9300A, M9301A and M9350A with improved stability and support for new memory module. "Drive BP 10MHz Reference" checkbox is added to M9391 SFP. This is equivalent of IVI-COM's Modules.Reference.BackPlaneReferenceEnabled property.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.1

Como Baixar

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

Como Instalar

  • Run the downloaded installer.

Licenciamento

  • Não Requer Licença

Documentação de suporte

2015-12-19 2.1.230.1 Fix interaction between applications using shared Reference or shared Synthesizer that may result in self test failures. Fix triggered multi-channel record mode with 89600 VSA Software.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.1

Como Baixar

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

Como Instalar

  • Run the downloaded installer.

Licenciamento

  • Não Requer Licença

Documentação de suporte

2015-08-20 2.1.221.0 Enhanced multichannel capability to support a maximum of 8 PXI VSAs in two chassis, including phase coherent operation with an LO distribution unit.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.0

Como Baixar

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

Como Instalar

  • Run the downloaded installer.

Licenciamento

  • Não Requer Licença

Documentação de suporte

2015-06-05 2.0.280.0 See description above.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.0

Version Description:

      Enhancements

  •  Updated help file, added IVI-2014 Compliance, rebranded as Keysight Technologies.
  • Added support for a maximum of 4 PXI VSAs in a single chassis sharing a single controller.
  • Improved multichannel timing synchronization performance.
     
  • Added phase synchronous operation via M9301A Synthesizer sharing capability, along with new IVI method and properties:
    - Calibration2.LOLevelAlignment.AlignLoLevel
    - Modulation3.BasebandPhase adjustment
    - Modules.Synthesizer3.SharedRole
    - Modules.Synthesizer.OutputPort
     
  • Added Reference3.AlignExternalReferenceAnd10MHzOut method to align phase of the 10 MHz Output with the External Reference input.
     

      Critical Fixes

  • Fix to enable using Modules.Reference.ProgrammableOutputTrigger properties when sharing M9300A Reference between multiple instruments.

Como Baixar

  1. Click the Download button.
  2. Choose Run.
     

Como Instalar

  • Run the downloaded installer.

Licenciamento

  • Não Requer Licença

Documentação de suporte

2015-01-14 1.2.417.1 See description above.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.0

Version Description:

  • Added features for 89600 VSA Software power spectrum measurements (Option 89601B-SSA):
    • Zero span measurements (power vs time)
    • Sweep trigger 
    • IF Magnitude trigger (for gating and sweep trigger)
    • Equivalent sweep time
    • Allow higher Span/RBW ratios when using a 64 bit process
    • Support M9000 resource manager sharing with multi-channel configurations
  • Fixture Loss tables are no longer cleared by ResetDefaultProperties() or Reset().
  • Fix to allow IF Filter alignment even when M9300A Reference module is not in the system timing slot.

Como Baixar

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

Como Instalar

  • Run the downloaded installer.

Licenciamento

  • Não Requer Licença

Documentação de suporte

2014-08-20 1.2.403.0 See description above.

Added support for 89600 VSA Software stepped spectrum measurement (Option 89601B-SSA). Added MultiChannelSync IVI interface and MultiChannel C# example to allow direct utilization of multi-channel capability. Previous 1.1.300.0 release offered multi-channel support via 89600 VSA software only. Improved speed performance. Eliminated AgModularVSA IVI interface. All functionality is now accessed directly via the AgM9391
interface. M9214A FPGA 1.0.2.3 available – Optional, not currently required for any new software features. M9300A FPGA 1.0.1.0 available – Optional, not currently required for any new software features. Fix allowing Modules.Reference.ProgrammableOutputTrigger properites to take effect. Fixed issue causing a ReadIQData() exception after running an IF Flatness alignment.

Note: This release is not binary compatible with prior releases of the IVI-C driver. Programs using the C/C++ IVI-C driver must be recompiled for this version of the driver. Similarly, programs compiled with this version of the driver will not be compatible with older versions of the IVI-C driver. This incompatibility is due to renumbering of attribute constants defined in
the AgM9391.h include file.

Como Baixar

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

Como Instalar

  • Run the downloaded installer.

Licenciamento

  • Não Requer Licença

Documentação de suporte

2013-11-01 1.1.300.0 Added multi-channel support via 89600 VSA software. Added FFT Acquisition Mode for faster power measurements. Fixes to improve Fixture Loss performance. Fixes IVI Config Store to remember options and "simulate" mode. Improved IF flatness calibration.

Como Baixar

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

Como Instalar

  • Run the downloaded installer.

Licenciamento

  • Não Requer Licença

Documentação de suporte

2013-08-30 1.0.69.0 Initial release.

Como Baixar

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

Como Instalar

  • See Documentation

Licenciamento

  • Não Requer Licença

Documentação de suporte