Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

34460A/34461A/34465A/34470A Firmware

Using the Keysight Firmware Update Utility, updates to the 34460A/34461A/34465A/34470A DMMs are available through the instrument’s LAN, GPIB, and USB IO ports, or front panel USB ‘host’ port.

Release Date Version Version Description
2017-11-22 2.17 Update to fix miscellaneous defects.

How to Download

  • Click the Download button.
    Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
    Unzip the file to access the .upd file. For updates using a front panel USB drive, the utility extracts the required files from the (unzipped) .upd file.

How to Install

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
  • It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

Licensing

  • Does Not Require a License

Supporting Documentation

Add-On Software / Utilities

Download

Installs on:

Instrument

Operating System

  • Windows 8
  • Windows 7
  • Windows Vista
  • Windows XP
  • Windows 10

Prerequisites

  • Prior to updating the firmware, 34460A/34461A/34465A/34470A DMMs with Security Option SEC must have the security feature unlocked. To unlock instrument security, press:
    Shift − Utility − Test/Admin – Security – Secure Code
    and enter the security code. The security feature can also be unlocked using the command:
    CALibration:SECurity:STATe OFF, security_code
    The factory-set security code is 'AT3446XA' For additional security this code may have been changed from its factory setting.
     

Supported Instruments

  • 34460A, 34461A, 34465A, 34470A
2016-04-27 2.14 Update to fix continuity tone on the 34460A/34461A, and accuracy issues following ACAL.

How to Download

  • Click the Download button.
    Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
    Unzip the file to access the .upd file. For updates using a front panel USB drive, the utility extracts the required files from the (unzipped) .upd file.

How to Install

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
  • It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

Licensing

  • Does Not Require a License

Supporting Documentation

Add-On Software / Utilities

Download

Installs on:

Instrument

Operating System

  • Windows 8
  • Windows 7
  • Windows Vista
  • Windows XP

Prerequisites

  • Prior to updating the firmware, 34460A/34461A/34465A/34470A DMMs with Security Option SEC must have the security feature unlocked. To unlock instrument security, press:
    Shift − Utility − Test/Admin ­ Security ­ Secure Code
    and enter the security code. The security feature can also be unlocked using the command:
    CALibration:SECurity:STATe OFF, security_code
    The factory-set security code is 'AT3446XA' For additional security this code may have been changed from its factory setting.

Supported Instruments

  • 34460A, 34461A, 34465A, 34470A