Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

34460A/34461A/34465A/34470A Firmware

Using the Keysight Firmware Update Utility, updates to the 34460A/34461A/34465A/34470A DMMs are available through the instrument’s LAN, GPIB, and USB IO ports, or front panel USB ‘host’ port.

Release Date Version Version Description
2020-02-12 3.02 Update to resolve memory leak.

How to Download

  • Click the Download button.
    Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
    Unzip the file to access the .upd file. For updates using a front panel USB drive, the utility extracts the required files from the (unzipped) .upd file.

How to Install

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
  • It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

Licensing

  • Does Not Require a License

Supporting Documentation

Add-On Software / Utilities

Download

Installs on:

Instrument

Operating System

  • Windows 8
  • Windows 7
  • Windows Vista
  • Windows XP
  • Windows 10

Prerequisites

  • * NOTICE: Downgrading the 3446xA and 34470A Firmware
    Before downgrading to a ‘Previous’ firmware revision, note the firmware revision currently installed (Shift - Help – About).
    Firmware revision A.03.01-02.40 and below can be downgraded to any previous (posted) revision.
    Firmware revision A.03.01-03.15 cannot be downgraded, and revisions above that can only be downgraded to A.03.01-03.15.
  • * NOTICE: Upgrading the 34460A and 34461A with firmware revision 1.xx to revision 3.0 or greater
    34460A and 34461A DMMs with firmware revision 1.08, 1.09, or 1.10 currently installed must first be upgraded to revision 2.17 (see the ‘Previous Versions’ tab), and then upgraded to revision 3.0 or greater. Upgrades to 3.0 or greater (from 1.xx) cannot be done directly. If attempted, the DMM can be recovered by updating the firmware (to 2.17) from the front panel USB port. Select ‘Front Panel’ on the Firmware Update Utility to create the appropriate folder on a USB thumb drive.
     

Supported Instruments

  • 34460A, 34461A, 34465A, 34470A