您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

EasyEXPERT group+ software (for PC)

New features, Resolved Issues and Revision History:
See Release Note.

Note:

  • This software is for new or update installation of EasyEXPERT group+ software (for PC).
  • Remote Control Interface is not supported on B150xA running on Windows XP.
  • From the revision 6.2.1927.7790, the Operating System must be Windows 7, Windows 8.1, or Windows 10 and Windows Vista is not supported.

License Requirement:
The license is required depending on how to use the software as follows.

  • Use without instrument
    The license is not required.
  • Use with B1500A/B1505A/B1506A/B1507A
    The license is not required.
  • Use with E5260A/E5262A/E5263A/E5270B/B2901A/B2902A/B2911A/B2912A
    One of the following license is required.
    B1500A(U)-SWS, B1505A(U)-SUS, B1506A-SWS, B1507A-SWS, E5260A(U)-SWS, E5270B(U)-SWS, B2901A(U)-SWS, B2902A(U)-SWS, B2911A(U)-SWS, B2912A(U)-SWS
     

EasyEXPERT group+ for PC; 6.2.1927.7790

發佈日期 版本 版本說明
2019-08-15 6.2.1927.7790 EasyEXPERT group+ for PC; 6.2.1927.7790
下載

安裝於:

PC

作業系統

  • Windows 7
  • Windows 8.1
  • Windows 10

必備檔案

  • See README file.

支援的儀器

  • B1500A,B1505A,B1506A,E5260A,E5262A,E5263A,E5270B,B2900A