Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

N9322C Spectrum Analyzer Firmware

Warning

Do not perform the firmware upgrade with an encrypted USB memory stick, which may cause unrecoverable hardware failure of the instrument.

Date de mise en circulation Version Description de la version
2017-06-28 A.06.27 The latest N9322C firmware revision

Comment télécharger

  1. Click the Download button
  2. Save file to PC.

Comment installer

  1. Extract files to the root directory of a USB stick. You will see a folder named N932xData with file N932XUPGRADE.PAC.
  2. Plug the USB disk in the USB connector on the top panel.
  3. Press [System] > {More} > {Service} > {Upgrade Firmware}, press [Enter] to upgrade the firmware. This procedure lasts about 10-15 mintues. Please keep power on and the USB disk connected. If the sceen is turned off, do not press power switch in 30 minutes.
  4. Unplug the USB disk and restart the unit when message

Autorisation d'exploitation

  • Ne requiert aucune licence

Document d'appui

Téléchargez

S'installe sur:

Instrument

Préalables

  • Information non-disponible

Instruments appuyés

  • N9322C