您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

Keysight Medalist i3070 08.30px Software Patches

System Requirements: Keysight Medalist i3070 test system or test development workstation
Controller Requirements: Windows ® PC
Operating System: Microsoft Windows ® 7 or Microsoft Windows ® XP
Software Requirement: Keysight Medalist i3070 08.30p

This software patch should only be installed on Microsoft Windows systems with Medalist i3070 08.30p software release. It can be installed on systems with i3070 test system software or i3070 development software.

Installing the 08.30px Software Patch

This software patch must be installed using the administrator login (or a login with administrator privileges).

Follow these steps to install the patch:

1. Save the Keysighti3070_08.30px.exe file to the hard disk.
2. Close all open programs.
3. Double- click Keysighti3070_08.30px.exe.
4. Follow the on- screen instructions for installation.
5. To validate that the software was installed correctly:
a. On the Start menu, select Programs > Keysight ICT > Korn Shell.
b. In the Korn Shell window, type version and press Enter.
The following software revision should be displayed:
Keysight Medalist i3070 08.30px 0612 WN.
 

* Windows registered trademarks of Microsoft Corporation.
 

發佈日期 版本 版本說明
2012-09-01 08.30pa Keysight Medalist i3070 08.30pa Software Patch

如何下載

  • 無相關資訊

如何安裝

  • 無相關資訊

授權

  • 不需要授權

支援文件

下載

安裝於:

PC

作業系統

  • Windows 7
  • Windows XP

必備檔案

  • 無相關資訊