这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

Keysight Medalist i3070 08.30px Software Patches

System Requirements: Keysight Medalist i3070 test system or test development workstation
Controller Requirements: Windows ® PC
Operating System: Microsoft Windows ® 7 or Microsoft Windows ® XP
Software Requirement: Keysight Medalist i3070 08.30p

This software patch should only be installed on Microsoft Windows systems with Medalist i3070 08.30p software release. It can be installed on systems with i3070 test system software or i3070 development software.

Installing the 08.30px Software Patch

This software patch must be installed using the administrator login (or a login with administrator privileges).

Follow these steps to install the patch:

1. Save the Keysighti3070_08.30px.exe file to the hard disk.
2. Close all open programs.
3. Double- click Keysighti3070_08.30px.exe.
4. Follow the on- screen instructions for installation.
5. To validate that the software was installed correctly:
a. On the Start menu, select Programs > Keysight ICT > Korn Shell.
b. In the Korn Shell window, type version and press Enter.
The following software revision should be displayed:
Keysight Medalist i3070 08.30px 0612 WN.
 

* Windows registered trademarks of Microsoft Corporation.
 

发布日期 版本 版本说明
2012-09-01 08.30pa Keysight Medalist i3070 08.30pa Software Patch

如何下载

  • 无此信息

如何安装

  • 无此信息

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 7
  • Windows XP

前提条件

  • 无此信息