Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

M938x Vector Signal Generator / CW Source Instrument Drivers

For a complete list of all IVI drivers from Keysight, please visit www.keysight.com/find/drivers

Release Date Version Version Description
2016-12-02 2.1.128.3 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0 

LabVIEW version: 2.0.1

Version details:

  • A new option string “BlankWhenArbPlaybackIsIdle” is added.
  • Fixed an intermittent glitch and/or jitter observed when playing an ARB with immediate or software trigger.
  • New FPGA bits with improved stability.
  • Fixes for intermittent issues with triggers and list mode.

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

2016-08-02 2.1.114.2 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0 

LabVIEW version: 2.0.1

Version details:

  • Fixed the issue of IQ swapping when loading MATLAB-generated complex data on M9381 SFP.
  • Fix to update the status of Modules.Reference.BackPlaneReferenceEnabled property correctly when the M9300A module is shared.
  • "Drive BP 10MHz Reference" checkbox is added to M9380 SFP and M9381 SFP. This is equivalent of IVI-COM's Modules.Reference.BackPlaneReferenceEnabled property.
  • Fix for LO Level alignment error when executing with option F03.
  • Fixed the logic to pick up the bit files available for firmware upgrade on M930x SFP.
  • Added capability to specify resources to be used in calibration (for Keysight Internal Use).

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

2016-01-28 2.1.87.1 Fixed interaction between applications using shared reference or shared synthesizer that resulted in self test errors. Fixed issue introduced in 1.4.405.1 which caused StartPlaybackOn10MHzClock synchronization to fail.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit)

IVI class support: IviDriver 1.0 

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

2015-08-19 2.1.85.0 Enhanced multichannel capability to support 8 PXI VSGs in two chassis, including phase coherent operation with a LO distribution unit. Added multichannel synchronized ArbRestart for up to 4 channels in a chassis. Added command :CALibration:LO:LEVel

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.01

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.
     

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

2015-05-23 2.0.333.0 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.01

Version Description:

Enhancements

  • Updated help file, added IVI-2014 Compliance, rebranded as Keysight Technologies.
  • Added support for a maximum of 4 PXI VSGs in a single chassis sharing a single controller.
  • Added MultiChannelSync IVI interface, enabling improved multichannel timing synchronization.
  • Added phase synchronous operation via M9301A Synthesizer sharing capability, along with new IVI method and properties:

         - Calibration2.LOLevelAlignment.AlignLoLevel

         - Modulation3.BasebandPhase adjustment

         - Modules.Synthesizer3.SharedRole

         - Modules.Synthesizer.OutputPort

  • Added Multichannel example program to demonstrate time and phase synchronous operation.
  • Added Reference3.AlignExternalReferenceAnd10MHzOut method to align phase of the 10 MHz Output with the External Reference input.
  • Added ArbMemory IVI interface to enable manual management of ARB memory usage.
  • Added Triggers.ExternalTrigger3.ArbRestart property.
  • l Enhanced SCPI interface with additional commands including multichannel operation.

Critical Fixes

  • Fix to enable using Modules.Reference.ProgrammableOutputTrigger properties when sharing M9300A Reference between multiple instruments.

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

2015-01-13 1.4.405.1 Fix to List mode operation with external trigger timeout enabled.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: M938x 1.0.14, M9300 1.06

How to Download

  • Click the download button and save the driver to your computer.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

2014-08-20 1.4.400.0 See description below.

Added SCPI interface with support for commonly used commands. Added support for Signal Studio 802.154g Wi-SUN. Improved speed performance. M9300A FPGA 1.0.1.0 available – Optional, not currently required for any new software features. Fix allowing Modules.Reference.ProgrammableOutputTrigger properites to take effect.
Fix to eliminate undesired Apply() performed within List.End() which previously could result in unintended signal output.

How to Download

  • Click the download button and save the driver to your computer.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

2013-11-01 1.3.300.0 See description below.

Added support for Signal Studio envelop tracking waveforms, N7624B-KFP(-KTP) and N7625B-KFP(-KTP). Expanded Synchronization Output Trigger functions to include the use of backplane triggers 0-7. M9311A Modulator FPGA updated to improve trigger jitter (FPGA version 1.0.0.4). Added external triggering delay capability (see Modulation2.BasebandDelay and Triggers2.ExternalTrigger2.Delay). Fix to improve Power Search accuracy. Fixes to improve Fixture Loss performance. Fixes IVI Config Store to remember options and "simulate" mode. Fix BackPlaneReferenceEnabled value to be unaffected by Reset.

How to Download

  • Click the download button and save the driver to your computer.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

2013-05-11 1.2.525.1 Fixes to prevent problem when the M9300 is shared by two or more instruments, prevent the RF power from being turned on unexpectedly in the learn phase of a List, shorten application startup time by disabling signature verification of the application

How to Download

  • Click the download button and save the driver to your computer.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP

Prerequisites

  • Information Not Available

Supported Instruments

  • M9380A, M9381A, M9301A, M9310A, M9311A, M9300A
2013-04-05 1.2.500.0 See release notes.

How to Download

  • Click the download button and save the driver to your computer.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP

Prerequisites

  • Information Not Available

Supported Instruments

  • M9380A, M9381A, M9301A, M9310A, M9311A, M9300A
2012-12-19 1.1.199.3 Corrected implementation of Nonvolatile that corrupted Nonvolatile contents. Changed the defaults of the Synchronization Output Trigger to be Enabled = true and Pulse Width = 10us.

How to Download

  • Click the download button and save the driver to your computer.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP

Prerequisites

  • Information Not Available

Supported Instruments

  • M9380A, M9381A, M9301A, M9310A, M9311A, M9300A
2012-11-28 1.1.196.2 Added self-test checks for more robust instrument error checking, miscellaneous cosmetic improvements to the Soft Front Panels for enhanced usability

How to Download

  • Click the download button and save the driver to your computer.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP

Prerequisites

  • Information Not Available

Supported Instruments

  • M9380A, M9381A, M9301A, M9310A, M9311A, M9300A
2012-09-30 1.1.186.1 Initial public release.

How to Download

  • Click the download button and save the driver to your computer.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP

Prerequisites

  • Information Not Available

Supported Instruments

  • M9380A, M9381A, M9301A, M9310A, M9311A, M9300A
2012-09-07 1.1.184.0

How to Download

  • Information Not Available

How to Install

  • Information Not Available

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP

Prerequisites

  • Information Not Available

Supported Instruments

  • M9380A, M9381A, M9301A, M9310A, M9311A, M9300A