您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

Keysight M938x 向量信號產生器 / 連續波信號源儀器驅動程式

如需查看是德科技所有 IVI 驅動程式的完整清單,請至 www.keysight.com/find/drivers

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0 

LabVIEW version: 2.0.1

Version details:

  • Windows 10 support
  • Support for new Signal Studio Licenses
  • In the previous release, intermittent glitch/jitter was fixed by adding zeros at the beginning of ARB. As this changes timing under a certain circumstance, we stop doing this as default. A new option string “ZeroPadding” is required to activate the feature.
發佈日期 版本 版本說明
2018-04-28 2.1.150.4 See description above.

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件