The N4980A Multi-Instrument BERT Software provides easy-to-use control panels for the following instruments:

Keysight Centellax
N4960A serial BERT 32 and 17 Gb/s SSB16000
N4962A serial BERT 12.5 Gb/s TG1B1A
N4963A clock synthesizer 13.5 Gb/s TG2C1A
N4965A multi-channel BERT 12.5 Gb/s PCB12500
N4971A pattern generator 13 Gb/s PPG12500
N4972A clock synthesizer 16 GHz SCS16000

N4980A-JTS jitter tolerance measurement package is an option enabled by a software key.

Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum Version Versionsbeschreibung
2015-02-18 3.3.2905 Adds support for Keysight branded instruments.
Veröffentlichungsdatum Version
2015-02-18 3.3.2905
Version Description
Adds support for Keysight branded instruments.

How to Download

  1. Click the Download button
  2. Save the software to your PC

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7 (32-bit) (English or Chinese)
  • Windows 7 (64-bit) (English)
  • Windows 10 (32-bit)
  • Windows 10 (64-bit)

Supported Instruments

  • N4960A, N4962A, N4963A, N4965A, N4971A, N4972A

How to Download

  1. Click the Download button
  2. Save the software to your PC

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7 32-bit (English or Chinese)
  • Windows 7 64-bit (English)

Voraussetzungen

  1. PC: Intel Pentium processor or equivalent
  2. Screen Resolution: XGA+ 1152x864 (min)
  3. RAM: 500 MB (min); 4 GB (min for Windows 7 64-bit)
  4. Disk space for installation: 100 MB
  5. .NET framework version 3.5
  6. I/O Libraries (for GPIB, not required for USB)

Supported Instruments

  • N4960A, N4962A, N4963A, N4965A, N4971A, N4972A

How to Download

  1. Click the Download button
  2. Save the software to your PC

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows XP 32-bit (with SP3)
  • Windows 7 32-bit (English or Chinese)
  • Windows 7 64-bit (English)

Voraussetzungen

  1. PC: Intel Pentium processor or equivalent
  2. Screen Resolution: 1024x768 (min)
  3. RAM: 500 MB (min)
  4. Disk space for installation: 100 MB

Supported Instruments

  • N4960A, N4962A, N4963A, N4965A, N4971A, N4972A

How to Download

  1. Download the software into the PC.
  2. Please read the N4980A Getting Started Guide before installing the software.

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows XP 32-bit (with SP3)
  • Windows 7 32-bit (English or Chinese)
  • Windows 7 64-bit (English)

Voraussetzungen

  1. PC: Intel Pentium processor or equivalent
  2. Screen Resolution: 1024x768 (min)
  3. RAM: 500 MB (min)
  4. Disk space for installation: 100 MB
  5. I/O Libraries

Supported Instruments

  • N4960A, N4962A, N4963A, N4965A, N4971A, N4972A

The N4980A is dependent upon low level Virtual Instrument Software Architecture (VISA), such as the Keysight I/O libraries. If the PC onto which the N4980A will be installed already has Keysight I/O libraries installed, then they do not need to be installed again.

For communicating with instruments via USB, the FTDI VCP driver must be installed. If this is not automatically installed by the Windows OS via Plug And Play, it must be manually installed by the user. The FTDI VCP driver can be found at www.ftdichip.com/Drivers/VCP.htm.

How to Download

  1. Download the software into the PC.
  2. Please read the N4980A Getting Started Guide before installing the software.

How to Install

  • See Documentation

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows XP 32-bit (with SP3)
  • Windows 7 32-bit (English or Chinese)
  • Windows 7 64-bit (English)

Voraussetzungen

  1. PC: Intel Pentium processor or equivalent
  2. Screen Resolution: 1024x768 (min)
  3. RAM: 500 MB (min)
  4. Disk space for installation: 100 MB
  5. I/O Libraries

Supported Instruments

  • N4960A, N4962A, N4963A, N4965A, N4971A, N4972A

The N4980A is dependent upon low level Virtual Instrument Software Architecture (VISA), such as the Keysight I/O libraries. If the PC onto which the N4980A will be installed already has Keysight I/O libraries installed, then they do not need to be installed again.

For communicating with instruments via USB, the FTDI VCP driver must be installed. If this is not automatically installed by the Windows OS via Plug And Play, it must be manually installed by the user. The FTDI VCP driver can be found at www.ftdichip.com/Drivers/VCP.htm.

How to Download

  1. Download the software into the PC.
  2. Please read the N4980A Getting Started Guide before installing the software.

How to Install

  • See Documentation

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows XP 32-bit (with SP3)
  • Windows 7 32-bit (English or Chinese)
  • Windows 7 64-bit (English)

Voraussetzungen

  1. PC: Intel Pentium processor or equivalent
  2. Screen Resolution: 1024x768 (min)
  3. RAM: 500 MB (min)
  4. Disk space for installation: 100 MB
  5. I/O Libraries

Supported Instruments

  • N4960A, N4962A, N4963A, N4965A, N4971A, N4972A

The N4980A is dependent upon low level Virtual Instrument Software Architecture (VISA), such as the Keysight I/O libraries. If the PC onto which the N4980A will be installed already has Keysight I/O libraries installed, then they do not need to be installed again.

For communicating with instruments via USB, the FTDI VCP driver must be installed. If this is not automatically installed by the Windows OS via Plug And Play, it must be manually installed by the user. The FTDI VCP driver can be found at www.ftdichip.com/Drivers/VCP.htm.

How to Download

  1. Download the software into the PC.
  2. Please read the N4980A Getting Started Guide before installing the software.

How to Install

  • See Documentation

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows XP 32-bit (with SP3)
  • Windows 7 32-bit (English or Chinese)
  • Windows 7 64-bit (English)

Voraussetzungen

  1. PC: Intel Pentium processor or equivalent
  2. Screen Resolution: 1024x768 (min)
  3. RAM: 500 MB (min)
  4. Disk space for installation: 100 MB
  5. I/O Libraries

Supported Instruments

  • N4960A, N4962A, N4963A, N4965A, N4971A, N4972A
SHOW MORE