Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Test Exec SL Version 7 Patches and Hotfixes

Test Exec SL Version 7 Software Updates

Patches and Hotfixes for Test Exec SL 7 Version 7

Release Date Version Version Description
2016-01-06 7.1.5 TestExec SL Version 7.1.5

This version of TestExec SL version 7.1.5 provides enhancements like:

1. enabling user to send a formatted string and data in operator user interface.

2. A new data log field of 'Unit Type' has been added. This field is automatically updated with result's unit type for an action.

3. An enhancement has been made to allow user to create / customize front panel in .NET.

4. An enhancement has been made in TestExec SL ActiveX Control and TestExec Core to introduce new property and method for checking an action is thread safe or non thread safe.

5. An enhancement has been made to display threaded test information such as test name, uut position name and sequence name for timeout thread at Main sequence, Waitthread, Testgroup, Local sequence and External sequence.

For full information of enhancements and bug fixes in this patch, please refer to the readme.txt file in the installation folder.

How to Download

  • Please click on the Download button to download the patch

How to Install

  • Please unzip the file and double click on the setup.exe file.

Licensing

  • Does Not Require a License
Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

Prerequisites

  • TestExec SL 7.1.1 must be installed first in order to apply the TestExec SL 7.1.5 patch.

Supported Instruments

  • TS-5040, TS-5020, TS-8989, TS-5400 PXI, TS-8900
2014-07-03 7.1.4 Test Exec SL 7.1.4 patch

Test Exec SL Version 7.1.4 patch contains patches and enhancements

How to Download

  • Click on the file link to download

How to Install

  • Unzip and run the TxSL_7.1.4_Patch.exe file

Licensing

  • Does Not Require a License
Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

Prerequisites

  • This version of TestExec SL 7.1.4 requires version 7.1.1 to be installed in the system.

Supported Instruments

  • TS-5040, TS-5020, TS-5400, TS-8900, TS-5400 PXI, TS-8989
2013-09-03 7.1.3 TestExec SL 7.1.3 enhancement details can be found in the file: readme - TxSL 7.1.3.txt

This TestExec SL version 7.1.3 includes enhancements.  For a full list of enhancements, please refer to readme - TxSL 7.1.3.txt file.

How to Download

How to Install

Licensing

  • Does Not Require a License
Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2
  • Windows XP

Prerequisites

Supported Instruments

  • TS-5040, TS-5020, TS-5400, TS-8900, TS-5400 PXI
2013-01-12 7.1.2 This new patch release incorporates new fixes and enhancements

This version of Test Exec SL encompasses further enhancements and bugfixes for version 7.1

How to Download

  • Click on the file link to download.

How to Install

  • Unzip and run the SETUP.EXE file.

Licensing

  • Does Not Require a License

Add-On Software / Utilities

Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows XP SP3
  • Windows XP SP2
  • Windows XP

Prerequisites

  • This version of patch requires Test Exec SL 7.1 installed in the system.

Supported Instruments

  • Not Applicable
2011-02-07 7.0.1 This new patch release incorporates new fixes and enhancements

How to Download

  • Click on download button.

How to Install

  • Unzip the downloaded file and run setup.exe file

Licensing

  • Does Not Require a License
Download

Installs on:

PC

Operating System

  • Windows XP
  • Windows XP SP2

Prerequisites

  • TestExec SL 7

Supported Instruments

  • Not Applicable