TS-5000 Version 7 Patches and Hotfixes for Windows 7 32-bit, Windows 7 64-bit and Windows XP 32-bit

Keysight는 가능한 최신 버전을 사용하는 것을 권장하며, 최신 버전에는 현재 사용 가능한 가장 최신 버그 수정 및 보안 패치가 포함되어 있습니다.
릴리스 날짜 버젼 버전 설명
2018-11-28 7.1.9 TS-5000 version 7.1 Service Pack 9
릴리스 날짜 버젼
2018-11-28 7.1.9
Version Description
TS-5000 version 7.1 Service Pack 9

Release summary:

  • Bug fix for detecting invalid/defective load card in SysConfig.exe. It will show unknown when defective load cards are detected.
  • Update test limit for VI in CEDGN U8989A.tpa and CEDGN U8972A.tpa.
  • Action Enhancement: Widen speed and resolution selection for M918x DMM’s dmeasdcv.umd action
     

다운로드 방법

  • Please click on the Download button to download the patch.

설치 방법

  • Please double click on the file setup.exe or right click the file setup.exe and select run

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7 32-bit
  • Windows 7 64-bit
  • Windows XP 32-bit

선결 조건

  • Information Not Available

지원되는 계측기

  • Entire TS-5400 family includes TS-5020, TS-5030, TS-5400 PXI, TS-5400, TS-5410, and TS-8989

The TS-5000 libraries version 7.1 Service Pack 8 is mainly for Keysight rebrand and added few instrument in our library and. For full details, please refer to the ReadMe.txt in the installation folder.

다운로드 방법

  • Please click on the Download button to download the patch.

설치 방법

  • Please double click on the file setup.exe or right click the file setup.exe and select

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7 32-bit
  • Windows 7 64-bit
  • Windows XP 32-bit

선결 조건

  • TestExec SL ver. 7.1.4 (or greater) must be installed prior to the installation of this patch.

지원되는 계측기

  • Entire TS-5400 family includes TS-5020, TS-5030, TS-5400 PXI, TS-5400, TS-5410, and TS-8989

The TS-5000 libraries version 7.1.5 patch contains enhancements and bug fixes.  For full details, please refer to the ReadMe.txt in the installation folder.

다운로드 방법

  • Please click on the Download button to download the patch.

설치 방법

please double click on the file setup.exe or right click the file setup.exe and select

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

선결 조건

  • TestExec SL ver. 7.1.3 and TS-5000 ver. 7.1.0 or 7.1.1 must be installed prior to the installation of this patch.

지원되는 계측기

  • TS-5040, TS-5020, TS-8989, TS-8900, TS-5400 PXI, TS-5400

The TS-5000 libraries version 7.1.4 patch contains enhancements and bug fixes.  For full details, please refer to the readme.txt in the installation folder.

다운로드 방법

  • Please click on the Download button to download the patch.

설치 방법

  • please double click on the file setup.exe or right click the file setup.exe and select

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

선결 조건

  • Test Exec SL version 7.1.3 and TS-5000 libraries version 7.1.0 must be installed prior to TS-5000 libraries version 7.1.4 installed.

지원되는 계측기

  • TS-5040, TS-5020, TS-5400, TS-8900, TS-5400 PXI, TS-8989

This TS-5000 libraries version 7.1.3 includes patches and enhancements.  For full details of the patches and enhancements, please refer to the ReadMe.txt in the TS5000 7.1 Service Pack 3.zip file.

다운로드 방법

  • Click on the download button.

설치 방법

  • Extract the zip file downloaded and run the Setup.exe file

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2
  • Windows XP

선결 조건

  • Information Not Available

지원되는 계측기

  • TS-5040, TS-5020, TS-5400, TS-8900, TS-5400 PXI

This TS-5000 libraries version 7.1.2 provides enhancements and bug fixes. For more details on the enhancements and bug fixes, please refer to the Readme file inside the installer

다운로드 방법

  • Click on the download button.

설치 방법

  • Unzip the file TS5000_7.1_ServicePack2.zip and run setup.exe

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7
  • Windows XP SP3
  • Windows XP SP2
  • Windows XP

선결 조건

  • Please install TS-5000 7.1.0V or TS-5000 7.1.1.1V prior to installing TS-5000 7.1.2v. �Please do not apply TS-5000 7.x Hotfix patch after installing TS-5000 7.1.2
    This service pack includes files for 7.x Hotfix.

지원되는 계측기

  • Not applicable

다운로드 방법

  • Click on download button.

설치 방법

  • Unzip downloaded file and run setup.exe.

라이센스

  • Does Not Require a License

Minor Updates

Installs on: PC

운영 체제

  • Windows 7

선결 조건

  • TS 5000 7

지원되는 계측기

  • Not Applicable

다운로드 방법

  • Click on download button.

설치 방법

  • Unzip downloaded file and run setup.exe.

라이센스

  • Does Not Require a License

Minor Updates

Installs on: PC

운영 체제

  • Windows 7

선결 조건

  • TS 5000 7

지원되는 계측기

  • Not Applicable
SHOW MORE