Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

TS-5000 Version 7 Patches and Hotfixes

TS-5000 Version 7 Patches and Hotfixes for Windows 7 32-bit, Windows 7 64-bit and Windows XP 32-bit

Release Date Version Version Description
2018-10-23 7.1.8 TS-5000 version 7.1 Service Pack 8

The TS-5000 libraries version 7.1 Service Pack 8 is mainly for Keysight rebrand and added few instrument in our library and. For full details, please refer to the ReadMe.txt in the installation folder.

How to Download

  • Please click on the Download button to download the patch.

How to Install

  • Please double click on the file setup.exe or right click the file setup.exe and select

Licensing

  • Does Not Require a License
Download

Installs on:

PC

Operating System

  • Windows 7 32-bit
  • Windows 7 64-bit
  • Windows XP 32-bit

Prerequisites

  • TestExec SL ver. 7.1.4 (or greater) must be installed prior to the installation of this patch.

Supported Instruments

  • Entire TS-5400 family includes TS-5020, TS-5030, TS-5400 PXI, TS-5400, TS-5410, and TS-8989
2016-05-12 7.1 Service Pack 6 TS-5000 version 7.1 Service Pack 6

The TS-5000 libraries version 7.1 Service Pack 6 is mainly for Keysight rebrand and added few instrument in our library and. For full details, please refer to the ReadMe.txt in the installation folder.

How to Download

  • Please click on the Download button to download the patch.

How to Install

  • Please double click on the file setup.exe or right click the file setup.exe and select

Licensing

  • Does Not Require a License
Download

Installs on:

PC

Operating System

  • Windows 7 32-bit
  • Windows 7 64-bit
  • Windows XP 32-bit

Prerequisites

  • TestExec SL ver. 7.1.4 (or greater) must be installed prior to the installation of this patch.

Supported Instruments

  • Entire TS-5400 family includes TS-5020, TS-5030, TS-5400 PXI, TS-5400, TS-5410, and TS-8989
2016-01-19 7.1.5 TS-5000 version 7.1.5 patch

The TS-5000 libraries version 7.1.5 patch contains enhancements and bug fixes.  For full details, please refer to the ReadMe.txt in the installation folder.

How to Download

  • Please click on the Download button to download the patch.

How to Install

  • please double click on the file setup.exe or right click the file setup.exe and select

Licensing

  • Does Not Require a License
Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

Prerequisites

  • TestExec SL ver. 7.1.3 and TS-5000 ver. 7.1.0 or 7.1.1 must be installed prior to the installation of this patch.

Supported Instruments

  • TS-5040, TS-5020, TS-8989, TS-8900, TS-5400 PXI, TS-5400
2014-11-14 7.1.4 TS-5000 libraries version 7.1.4 patch

The TS-5000 libraries version 7.1.4 patch contains enhancements and bug fixes.  For full details, please refer to the readme.txt in the installation folder.

How to Download

  • Please click on the Download button to download the patch.

How to Install

  • please double click on the file setup.exe or right click the file setup.exe and select

Licensing

  • Does Not Require a License
Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

Prerequisites

  • Test Exec SL version 7.1.3 and TS-5000 libraries version 7.1.0 must be installed prior to TS-5000 libraries version 7.1.4 installed.

Supported Instruments

  • TS-5040, TS-5020, TS-5400, TS-8900, TS-5400 PXI, TS-8989
2013-10-17 7.1.3 TS-5000 libraries version 7.1.3 patches and enhancement details can be found in the file: Readme.txt in the zip file

This TS-5000 libraries version 7.1.3 includes patches and enhancements.  For full details of the patches and enhancements, please refer to the ReadMe.txt in the TS5000 7.1 Service Pack 3.zip file.

How to Download

  • Click on the download button.

How to Install

  • Extract the zip file downloaded and run the Setup.exe file

Licensing

  • Does Not Require a License
Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2
  • Windows XP

Prerequisites

  • Information Not Available

Supported Instruments

  • TS-5040, TS-5020, TS-5400, TS-8900, TS-5400 PXI
2013-03-08 7.1.2 TS-5000 libraries ver. 7.1.2

This TS-5000 libraries version 7.1.2 provides enhancements and bug fixes. For more details on the enhancements and bug fixes, please refer to the Readme file inside the installer

How to Download

  • Click on the download button.

How to Install

  • Unzip the file TS5000_7.1_ServicePack2.zip and run setup.exe

Licensing

  • Does Not Require a License
Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows XP SP3
  • Windows XP SP2
  • Windows XP

Prerequisites

  • Please install TS-5000 7.1.0V or TS-5000 7.1.1.1V prior to installing TS-5000 7.1.2v. �Please do not apply TS-5000 7.x Hotfix patch after installing TS-5000 7.1.2
    This service pack includes files for 7.x Hotfix.

Supported Instruments

  • Not applicable
2012-05-25 7.1 Service Pack 1.1 This service pack incorporates new actions and handlers for additional instruments within the TS series functional test systems plus some bugfixes. This service pack is meant for TS-5000 version 7.1 only

How to Download

  • Click on download button.

How to Install

  • Unzip downloaded file and run setup.exe.

Licensing

  • Does Not Require a License

Hotfixes / Software Patches

Download

Installs on:

PC

Operating System

  • Windows 7

Prerequisites

  • TS 5000 7

Supported Instruments

  • Not Applicable
2011-01-18 7.0.1 Patch The TS-5000 7.0.1 software supports the entire TS5000 family which includes TS5400, TS5410, TS5020, TS5030. This version includes multi-threading capability to handlers and bugfixes. Refer to readme.tzt for details

How to Download

  • Click on download button.

How to Install

  • Unzip downloaded file and run setup.exe.

Licensing

  • Does Not Require a License

Hotfixes / Software Patches

Download

Installs on:

PC

Operating System

  • Windows 7

Prerequisites

  • TS 5000 7

Supported Instruments

  • Not Applicable