Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

IO Libraries Suite Downloads

To find out more about the IO Libraries Suite, visit www.keysight.com/find/iosuite

Choose a platform:

IO Libraries Suite 2020 Update 1 offers two significant changes from the previous software version:

  • It fixes the discovery process for the 1394-VXI interface when the VXI system is using MXI connections.
  • It fixes the memory leaking issues in the Keysight Instrument Discovery Service and LxiMdnsBrowser.

The remaining enhancements in this list were made for IO Libraries Suite 2020.

  • General performance enhancements.
  • VISA Shared Components - Upgrade to 5.12.
  • Support for GPIB drivers with Windows 10 Device Guard.
  • Bug fixes and minor enhancements including:
    • When NI is the primary resource manager, Connection Expert now reports all NI PXI modules.
    • On systems with NI VISA, an install repair operation completes fully.
    • When the NI PXI system module is used with Keysight Resource Manager as the primary resource manager, the full address of the system module is now reported correctly.
    • Serial instrument detection is fixed.
    • Following an upgrade, the GPIB instrument list is properly refreshed.
    • Checking status on a LAN instrument completes without interrupting instrument discovery.
    • Serial ports, which were not displaying in Connection Expert in certain configurations, are now visible.
    • Following an upgrade, the GPIB instrument list is properly refreshed.
    • Checking status on a LAN instrument completes without interrupting instrument discovery.
    • Serial ports, which were not displaying in Connection Expert in certain configurations, are now visible.
Release Date Version Version Description
2020-10-15 2020 Update 1 See description above. Build 18.1.26209.5

How to Download

  • Click the download link and save the installer.

How to Install

  • Run the downloaded installer with Admin Privilege.

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 10 v1809 and above
  • Windows 8.1 Enterprise
  • Windows 7 SP1 Enterprise

Prerequisites

  • For Windows 10: .NET Framework 3.5/2.0 installed

Related Links