Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

New Bootpt.exe file for i3070

You can install a newer version of BOOTP Turbo software to resolve the boot issue.

Installation Procedure:

1. Download the “bootpt.exe”.
2. Back up the bootptab file in c:\Windows\system32\drivers\etc by renaming it to bootptab.org.
3. Go to Control Panel > Programs and Features, Remove BOOTP Turbo software
4. To install the newer version, double click on “bootpt.exe”
5. Follow the instruction to complete the installation.
6. Rename bootptab.org to bootptab in c:\Windows\system32\drivers\etc.
7. Restart the PC.

*Microsoft and Windows are trademarks or registered trademarks of Microsoft Corporation in the United States and/or other countries.

Date de mise en circulation Version Description de la version
2013-03-15 Control_XTPA New Bootp file to solve the intermittent boot error with “Control XTPA” (N1807-66801) on Windows ® 7, software version 08.30pb.

Problem Description:

An intermittent boot error might occur with the i3070 Control XTPA card on Win 7 systems running software version 08.30pb.

If boot service is being restarted, some systems may intermittently encounter this boot problem.

This problem usually goes away with subsequent re-boots.

Note: You don't have to install this bootp installer if you do not encounter any boot error as mentioned above.

Please refer to Service Note 3070-89 for details.

Comment télécharger

  • Information non-disponible

Comment installer

  • Information non-disponible

Autorisation d'exploitation

  • Ne requiert aucune licence
Téléchargez

S'installe sur:

PC

Système d'exploitation

  • Windows 7
  • Windows XP

Préalables

  • Information non-disponible

Instruments appuyés

  • i3070