이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

Firmware update for U1271A & U1272A Handheld Digital Multimeter - Rev 2.04

Always update your handheld digital multimeters with the latest firmware to maximize the performance of the instrument.

릴리스 날짜 버젼 버전 설명
2015-09-21 3.03 Firmware update for U1271A & U1272A.

다운로드 방법

  • 1. Connect the multimeter to your PC via the U1173B IR-USB connectivity cable and turn on the multimeter.
    2. Go to Start>All Programs>Keysight Technologies>Keysight U1271A U1272A Firmware Update>Keysight U1271A U1272A Firmware Update Software (version 3.03).
    3. Click Auto Search COM Port button to search and detect the unit. The model number, serial number and current firmware version of the multimeter will be displayed in the Model Number, Serial Number and Current Version field.
    4. Make sure the instrument is in connected status before you start firmware update. Click. Upload Firmware to start firmware update.
    5. The multimeter will reset and recover itself after the firmware update.
    6. Reset the multimeter to its Default values through the setup menu (refer to User Guide page 150). This step is mandatory.

설치 방법

  • Installing the software:
    1. Unzip the zip file to a folder.
    2. Go to folder PL2303_XPVistaWin7_Driver, click on the PL2303_XPVistaWin7Driver.exe to install the U1173B IR-USB cable driver.
    3. Double click the Setup.exe file to install the program.
  • Uninstalling the software:
    1. Go to Start>Control Panel, then double click Add or Remove Programs.
    2. In the Currently installed progrms window, select the program that you want to remove, then click Remove.

라이센스

  • 라이센스 필요 없음

지원 문서

다운로드

설치 위치:

Instrument

운영 체제

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows 2000

사전 조건

  • System Requirements: Intel Pentium 4, 1 GHz or equivalent, 512 MB RAM, 1 GB HDD free space.

지원되는 계측기

  • U1271A, U1272A