Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

M950xA AXIe Chassis Drivers

This driver installs the IVI-C, IVI-COM, LabVIEW, and MATLAB driver components, as well as the soft front panel and kernel device driver.
 

For a complete list of all IVI drivers from Keysight, please visit www.keysight.com/find/drivers


 

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), Labview (32-bit/64-bit), MATLAB (32-bit only)
 

IVI class support: IviDriver 1.0

Date de mise en circulation Version Description de la version
2017-09-20 1.4.2.1 Added support for Windows 8.1 and Windows 10. Changed to allow AXIe chassis to be detected correctly in Keysight IO Libraries when modules with multiple PCIe endpoints are inserted.

Comment télécharger

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

Comment installer

  • Run the downloaded installer.

Autorisation d'exploitation

  • Ne requiert aucune licence

Document d'appui