您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

Base - X-Series Signal Analyzers IVI and MATLAB Instrument Drivers

 

Not the driver you were looking for? See all Signal Analyzer Instrument drivers at:

https://www.keysight.com/find/sa-ivi

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

發佈日期 版本 版本說明
2018-07-31 3.5.7.0 Defect fix

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0
 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

下載

安裝於:

PC

作業系統

  • Windows 8
  • Windows 7
  • Windows 10

必備檔案

支援的儀器

  • N9000A, N9000B, N9010A, N9010B, N9020A, N9020B, N9030A, N9030B, N9038A, M9290A, N9040B, N9041B, M9420A, M9421A, PN9003A, SPN9026A, N8973B, N8974B, N8975B, N8976B, M90XA, M8920A

相關連結

2018-05-26 3.5.6.0 Added support for M8920A

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0
 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

下載

安裝於:

PC

作業系統

  • Windows 8
  • Windows 7
  • Windows 10

必備檔案

支援的儀器

  • N9000A, N9000B, N9010A, N9010B, N9020A, N9020B, N9030A, N9030B, N9038A, M9290A, N9040B, N9041B, M9420A, M9421A, PN9003A, SPN9026A, N8973B, N8974B, N8975B, N8976B, M90XA, M8920A

相關連結

2017-09-21 3.5.2.0 Adds support for M90XA. Updated to be compatible with firmware 19.05 and later.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0
 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2017-03-07 3.4.2.0 Added support for N9041B, added System Preset, Global Center Freq, Extended Low Band, and External Trigger Compensation functionality. Fixed an issue where the driver would fail to install if the help file could not be installed.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0
 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2016-06-02 3.3.0.0 Adds support for the M9421A.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0
 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2016-01-05 3.2.3.0 Model support added for N9000B,N9010B, N9020B, N9030B, SPN9003A, SPN9026A, N8973B, N8974B, N8975B, N8976B.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0
 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.
     

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

下載

安裝於:

PC

作業系統

  • Windows 8
  • Windows 7
  • Windows Vista
  • Windows XP

必備檔案

支援的儀器

  • N9000A N9000B N9010A N9010B N9020A N9020B N9030A N9030B N9038A M9290A N9040B M9420A SPN9003A SPN9026A N8973B N8974B N8975B N8976B

相關連結

2015-11-03 3.1.2.0 Implementation of IAgXSAnSystem.GetScreenImage method is modified to store the Screen.png file at D: incase of firmware version A.14 or earlier and to C:Temp incase of firmware version A.15 and later.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2015-10-28 3.1.1.0 See description above.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0

Version description:

  • Customer issue fixed by changing the implementation of IAgXSAnInputRf.Coupling, removed the option checking and made equivalent to version before 3.0.0.0. Any option issue would be reported as error.
  • Customer issue fixed by changing the implementation logic of the IAgXSAnCalibration.Calibrate() method to read the status of calibration before returning, and increased the timeout to 240 seconds to cater to any delays or long calibration turnaround time.
  • Modified the implementation logic of the Initialze method for M9420A and M9290A modules, in case of PXI address, it check for module name and then take the correct installation path of LaunchModularSA.exe path based on the module name.
  • IVI-C issue fixed for some functions which take a Null value as an input.
  • Implementation of IAgXSAnSystem.GetScreenImage method is modified to remove the D: drive from the path.
  • Added trace numbers from 13 to 17 in SEMAsk measurement. Now user can access traces from 13 to 17.
     

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.
     

如何安裝

  • Run the downloaded installer

授權

  • 不需要授權

支援文件

2015-07-21 3.1.0.0 Added support for M9420A.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.
     

如何安裝

  • Run the downloaded installer

授權

  • 不需要授權

支援文件

2015-04-18 3.0.0.0 Tracking Generator support added to N9000A and M9290A models.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0
 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer

授權

  • 不需要授權

支援文件

2014-11-21 2.2.1.0 Rebranded Keysight Technologies, added support of UXA (N9040B) and CXA-m (M9290A).

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0

IVI Generation: IVI-2014

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

如何安裝

  • Run the downloaded installer

授權

  • 不需要授權

支援文件

2014-04-26 2.1.4.0 Changed the implementation of the IAgXSAnCalibration.Calibrate method to increase the timeout of :CALibration[:ALL] SCPI.

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

如何安裝

  • Run the downloaded installer

授權

  • 不需要授權

支援文件

2014-01-06 2.1.3.0 Fixed an application crash when calling init function (IVI-COM or IVI-C) if you use an address where there is no instrument available (e.g. instrument is turned off or LAN cable is disconnected).

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

如何安裝

  • Run the downloaded installer

授權

  • 不需要授權

支援文件

2013-06-26 2.1.2.0 Defect fixes and system interface revised for adding ClearIO, ReadByte(),WriteByte(),ReadString(),WriteString() methods

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

如何安裝

  • Run the downloaded installer

授權

  • 不需要授權

支援文件

2011-05-24 2.0.0.0 Applied updated policy. No functionality change.

如何下載

  • 1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Run.

如何安裝

  • See Readme File

授權

  • 不需要授權

支援文件

2011-05-10 1.0.5.0 Initial public release.

如何下載

  • 1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Run.

如何安裝

  • See Readme File

授權

  • 不需要授權

支援文件