이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

PXIe 섀시 제품군 드라이버

키사이트의 모든 계측기 드라이버 전체 목록 확인: www.keysight.com/find/drivers

참고: 설정에서 시스템 모듈을 사용하는 경우 시스템이 제대로 작동하게 하려면 M902x PXIe 시스템 모듈 드라이버도 설치해야 합니다.

릴리스 날짜 버젼 버전 설명
2017-04-19 1.6.493.1 See description below.

Changes in release 1.6.493.1:

  • Added support for two new Gen3 PXIe Chassis: the 10 slot M9010A and the 18 slot M9019A.

With the addition of these two new PXIe Chassis to the Chassis Family, four chassis are now supported.

  • Added the Keysight Technologies Trigger Manager driver (KtMTrig) to provide an enhanced API (IVI.NET and IVI-C) for making reservations and setting trigger routes on the PXIe Chassis backplane.

With the addition of the Trigger Manger driver, this installer now provides the 3 drivers listed below.

  • Fixed various defects to improve the reliability of PCIe device boot time enumeration.
  • Fixed a defect so the Soft Front Panel can run if the OS language format is set to a value other than English.
  • Changed the default minimum fan speed for the M9010A from 1200 RPM to 900 RPM.
  • Added additional example programs to demonstrate control of Front Panel Trigger Ports and how to use the Trigger Manager.
  • Added a feature to flash LEDs on the chassis front panel for identifying M9010A, M9018B, and M9019A.
  • Enhanced the Soft Front Panel to make it easier to use and included:
  • Display of PCIe link speed and number of lanes for M9010A and M9019A.
  • Display of alarm notification on tab label.

This installer contains 3 drivers:

KtMPxiChassis Driver

  • PXIe Chassis Family driver
  • IVI.NET and IVI-C API
  • See introduction file for additional information

KtMTrig driver

  • Trigger Manager
  • IVI.NET and IVI-C API
  • See introduction file for additional information

AgM9018 Driver

  • Legacy M9018A driver to support applications written for version 1.5.80.1 of AgM9018 driver
  • IVI-C and IVI-COM API
  • See introduction file for additional information

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.
     

라이센스

  • 라이센스 필요 없음

지원 문서

2016-09-04 1.6.2.1 See description below.

This package installs 2 drivers:

KtMPxiChassis Driver

  • Driver type: IVI-C (32-bit/64-bit), IVI.NET (32-bit/64-bit), LabVIEW (32-bit/64-bit)
  • IVI-C class support: IviDriver 2.1
  • IVI.NET class support: IviDriver 1.0
  • LabVIEW driver version: 1.0.1
  • Version description:
    • Initial release
    • Supports M9019A

Legacy AgM9018 Driver

  • Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)
  • IVI class support: IviDriver 1.0
  • LabVIEW driver version: 1.1.5
  • Version description:
    • New feature added: Trigger Manager for managing trigger resources to prevent conflicts between applications. The AgM9018 IVI driver API has not changed, however, trigger routing done through the AgM9018 driver is now subject to PXI-9 Trigger Manager rules which can result in errors indicating a conflict between applications.
    • Supports M9018A

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • 라이센스 필요 없음

지원 문서

2015-02-05 1.5.80.1 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.2.6

Version description:

  • Changes made to support the HP Z440/640/840 series of controllers
  • Visual Studio examples updated to use Visual Studio 2010 (or later)
  • Document changes to meet IVI-2014 Compliance
  • Rebranded as Keysight Technologies

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • 라이센스 필요 없음

지원 문서

2014-10-28 1.4.397.1 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.0.5

Version description:

  • Updated to Rev 2 of 2x8 and 4x4 PCIe fabrics.
  • Default fan alarm level raised from 800 rpm to 1200 rpm.
  • Eliminated use of English-language dependent string in System Module DLL.
  • Eliminated driver 1st-contact SMBus self test operations to improve interoperability.

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • 라이센스 필요 없음

지원 문서

2013-07-19 1.3.443.1 Updated PXI System Module DLL and Chassis Driver DLL to support cascaded multi-chassis systems. Added 1x8 PCIe Gen1 speed fabric to PCIe Switch Fabric Configurator (for use with multi-chassis systems).

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

설치 방법

  • Run the downloaded installer.
  • If you see a Windows Security prompt, check the box Always trust software from "Agilent Technologies, Incorporated", then click the Install button to install the driver.

라이센스

  • 라이센스 필요 없음

지원 문서

2012-03-22 1.2.3 Added support for 2-Link 2x8 PCIe Switch Fabric, added support for Keysight IO Libraries 16.2, fixed assorted PXI compliance issues (updated System Module DLL, Chassis DLL, and Chassis Description file)

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

설치 방법

  • Run the downloaded installer.
  • If you see a Windows Security prompt, check the box Always trust software from "Agilent Technologies, Incorporated", then click the Install button to install the driver.

라이센스

  • 라이센스 필요 없음

지원 문서

2011-03-07 1.0.3 M9018A Driver Version 1.0.3 for 18 Slot PXIe Chassis

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.
  • If you see a Windows Security prompt, check the box Always trust software from "Agilent Technologies, Incorporated", then click the Install button to install the driver.
     

라이센스

  • 라이센스 필요 없음

지원 문서