PXIe 섀시 제품군 드라이버
키사이트의 모든 계측기 드라이버 전체 목록 확인: www.keysight.com/find/drivers
참고: 설정에서 시스템 모듈을 사용하는 경우 시스템이 제대로 작동하게 하려면 M902x PXIe 시스템 모듈 드라이버도 설치해야 합니다.
Changes in release 1.7.82.1:
-
Enhanced the capability of the front panel Trigger Ports.
Notice:
To gain this enhanced capability, the chassis firmware must be updated to version 2018.
The 1.7.82.1 PXIe Chassis family driver will work with both the 2017 firmware and the 2018 firmware.
Older versions of the driver will only work with the 2017 firmware.
The enhanced capability allows you to:
• Configure a front panel Trigger Port to Input and connect to multiple PXI_TRIG signal lines on two Trigger Bus Segments.
• Configure a front panel Trigger Port to Output and connect to a single PXI_TRIG signal line on either of two Trigger Bus Segments.
See the User Guide for details. -
Fixed various defects to improve reliability and quality.
This installer contains 3 drivers:
KtMPxiChassis Driver
- PXIe Chassis Family driver
- IVI.NET and IVI-C API
- See introduction file for additional information
KtMTrig driver
- Trigger Manager
- IVI.NET and IVI-C API
- See introduction file for additional information
AgM9018 Driver
- Legacy M9018A driver to support applications written for version 1.5.80.1 of AgM9018 driver
- IVI-C and IVI-COM API
- See introduction file for additional information
릴리스 날짜 | 버젼 | 버전 설명 |
---|---|---|
2018-08-16 | 1.7.82.1 | See description above. |
다운로드 방법
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
설치 방법
- Run the downloaded installer for version 1.7.82.1.
라이센스
- 라이센스 필요 없음
지원 문서
다운로드
설치 위치:
PC
운영 체제
- Windows 7
- WES 7
- Windows 8.1
- Windows 10
사전 조건
지원되는 계측기
- M9010A, M9018A, M9018B, M9019A