Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

PXIe Chassis Family Drivers

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

Note: If you use the system module in your setup, you’ll need to also install the M902x PXIe System Module Driver in order to get your system to work properly.

Release Date Version Version Description
2017-04-19 1.6.493.1 See description below.

Changes in release 1.6.493.1:

  • Added support for two new Gen3 PXIe Chassis: the 10 slot M9010A and the 18 slot M9019A.

With the addition of these two new PXIe Chassis to the Chassis Family, four chassis are now supported.

  • Added the Keysight Technologies Trigger Manager driver (KtMTrig) to provide an enhanced API (IVI.NET and IVI-C) for making reservations and setting trigger routes on the PXIe Chassis backplane.

With the addition of the Trigger Manger driver, this installer now provides the 3 drivers listed below.

  • Fixed various defects to improve the reliability of PCIe device boot time enumeration.
  • Fixed a defect so the Soft Front Panel can run if the OS language format is set to a value other than English.
  • Changed the default minimum fan speed for the M9010A from 1200 RPM to 900 RPM.
  • Added additional example programs to demonstrate control of Front Panel Trigger Ports and how to use the Trigger Manager.
  • Added a feature to flash LEDs on the chassis front panel for identifying M9010A, M9018B, and M9019A.
  • Enhanced the Soft Front Panel to make it easier to use and included:
  • Display of PCIe link speed and number of lanes for M9010A and M9019A.
  • Display of alarm notification on tab label.

This installer contains 3 drivers:

KtMPxiChassis Driver

  • PXIe Chassis Family driver
  • IVI.NET and IVI-C API
  • See introduction file for additional information

KtMTrig driver

  • Trigger Manager
  • IVI.NET and IVI-C API
  • See introduction file for additional information

AgM9018 Driver

  • Legacy M9018A driver to support applications written for version 1.5.80.1 of AgM9018 driver
  • IVI-C and IVI-COM API
  • See introduction file for additional information

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.
     

Licensing

  • Does Not Require a License

Supporting Documentation

2016-09-04 1.6.2.1 See description below.

This package installs 2 drivers:

KtMPxiChassis Driver

  • Driver type: IVI-C (32-bit/64-bit), IVI.NET (32-bit/64-bit), LabVIEW (32-bit/64-bit)
  • IVI-C class support: IviDriver 2.1
  • IVI.NET class support: IviDriver 1.0
  • LabVIEW driver version: 1.0.1
  • Version description:
    • Initial release
    • Supports M9019A

Legacy AgM9018 Driver

  • Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)
  • IVI class support: IviDriver 1.0
  • LabVIEW driver version: 1.1.5
  • Version description:
    • New feature added: Trigger Manager for managing trigger resources to prevent conflicts between applications. The AgM9018 IVI driver API has not changed, however, trigger routing done through the AgM9018 driver is now subject to PXI-9 Trigger Manager rules which can result in errors indicating a conflict between applications.
    • Supports M9018A

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

2015-02-05 1.5.80.1 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.2.6

Version description:

  • Changes made to support the HP Z440/640/840 series of controllers
  • Visual Studio examples updated to use Visual Studio 2010 (or later)
  • Document changes to meet IVI-2014 Compliance
  • Rebranded as Keysight Technologies

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

2014-10-28 1.4.397.1 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.0.5

Version description:

  • Updated to Rev 2 of 2x8 and 4x4 PCIe fabrics.
  • Default fan alarm level raised from 800 rpm to 1200 rpm.
  • Eliminated use of English-language dependent string in System Module DLL.
  • Eliminated driver 1st-contact SMBus self test operations to improve interoperability.

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

2013-07-19 1.3.443.1 Updated PXI System Module DLL and Chassis Driver DLL to support cascaded multi-chassis systems. Added 1x8 PCIe Gen1 speed fabric to PCIe Switch Fabric Configurator (for use with multi-chassis systems).

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

How to Install

  • Run the downloaded installer.
  • If you see a Windows Security prompt, check the box Always trust software from "Agilent Technologies, Incorporated", then click the Install button to install the driver.

Licensing

  • Does Not Require a License

Supporting Documentation

2012-03-22 1.2.3 Added support for 2-Link 2x8 PCIe Switch Fabric, added support for Keysight IO Libraries 16.2, fixed assorted PXI compliance issues (updated System Module DLL, Chassis DLL, and Chassis Description file)

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

How to Install

  • Run the downloaded installer.
  • If you see a Windows Security prompt, check the box Always trust software from "Agilent Technologies, Incorporated", then click the Install button to install the driver.

Licensing

  • Does Not Require a License

Supporting Documentation

2011-03-07 1.0.3 M9018A Driver Version 1.0.3 for 18 Slot PXIe Chassis

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.
  • If you see a Windows Security prompt, check the box Always trust software from "Agilent Technologies, Incorporated", then click the Install button to install the driver.
     

Licensing

  • Does Not Require a License

Supporting Documentation