这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

安装 InfiniiVision 3000 X 系列示波器固化软件

您可以在发布说明(文档和下载摂部分)中查看固化软件变化概要。

是德对 InfiniiVision X 系列示波器固化软件进行定期更新,以提供最新特性、采纳客户建议并确保适当的功能。您必须更新固化软件方可使用新特性。

要想查看示波器当前的固化软件版本,请按下前面板的 [Help] 键,然后按下 About Oscilloscope 功能键。

要想更新示波器的固化软件,请执行以下一种操作:

  • 将文件存放到 U 盘,并将该 U 盘连接到示波器,按下 [Utility] > File Explorer,选择该文件,然后按下 Load File
  • 如果示波器已联网:可将文件存放在计算机上,访问示波器的 Web 界面(查看《用户指南》获取详情),点击 Instrument Utilities,选择 Firmware Version,浏览并选择该文件,然后点击 Install。

更新示波器的固化软件之后,请检查其校准状态:按下 [Utility] > Service > User Cal Status。如果显示“Results: OK”,那么您无需进行重新校准。如果需要校准,请按下Start User Cal功能键。

发布日期 版本 版本说明
2019-03-08 2.50 This is the firmware for the 3000 X-Series oscilloscopes.

如何下载

  • Click the download button and save the file to a USB flash drive or to a temporary directory on your computer.
  • CAUTION: If your oscilloscope’s software version is prior to 2.41, you will need to change the suffix of the upgrade file from .ksx to .cab. Do not “unpack” or “unzip” the renamed .cab upgrade file; you could potentially load only a portion of the required files in the package, and this could result in your oscilloscope becoming non-operational, requiring it to be sent to a Keysight service center to be repaired.
  • If you are unable to SAVE the file, please try a different browser or contact us for help.

如何安装

  • To update your oscilloscope's firmware, do one of the following:
    • Place the file on a USB flash drive, connect it to the oscilloscope, press [Utility] > File Explorer, select the file; then, press Load File.
    • If your oscilloscope is on the network: you can place the file on your computer, access the oscilloscope's Web Interface (see the User's Guide for details), click Instrument Utilities, select Firmware Version, browse to select the file; then, click Install.
  • After your oscilloscope's firmware is updated, check the calibration status: press [Utility] > Service > User Cal Status. If "Results: OK" is displayed, you do not need to recalibrate. If calibration is required, press the Start User Cal softkey.

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

Instrument

前提条件

  • 无此信息

支持的仪器

  • MSOX3104A, DSOX3104A, MSOX3102A, DSOX3012A, MSOX3012A, DSOX3014A, MSOX3014A, DSOX3024A, MSOX3024A, DSOX3032A, MSOX3032A, DSOX3034A, MSOX3034A, DSOX3052A, MSOX3052A, DSOX3054A, MSOX3054A

相关链接