検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

N9038A MXE EMI Receiver Instrument Software

PLEASE NOTE:

  • Instruments running the Windows 7 and Windows 10 operating system - See the Current Version tab below
  • Instruments running the Windows XP operating system - See the Previous Versions tab below
  • There is no need to recalibrate when new instrument software is installed.

To determine the operating system installed refer to the certificate of authenticity (COA) on the rear panel of the instrument.

リリース バージョン 内容
2015-07-07 A.14.16 Downloadable installation file of the latest software version for instruments running the Windows XP operating system...

ダウンロード方法

  • If your receiver is connected to the network, download the software update package directly onto the receiver and run the file.
  • Otherwise, download the package onto your PC and transfer the file to the receiver using a USB storage device.
  • Note: Do not run the instrument software executable file on your personal computer. It must be run on the receiver being updated.

インストール方法

ライセンス

説明資料