Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

N9038A MXE EMI Receiver Instrument Software

PLEASE NOTE:

• Optional measurement applications will require a license with Software Support Expiration Date later than S/W Version Date listed below in Version Description to access the enhancements available for that application in this release. To check the Software Support Expiration Dates on your analyzer, press System, Show, Support Subscriptions. If the Software Support Expiration Status is listed as "Not Applicable" for a particular measurement application, that measurement application's features will be limited to what was available in the A.19.55 release.
• Instruments running the Windows 7 or Windows 10 operating system – Refer to both the Current Version and Previous Version tabs below.
• Instruments running the Windows XP operating system – See the Previous Versions tab below
• There is no need to recalibrate when new instrument software is installed.
 

Date de mise en circulation Version Description de la version
2020-07-09 A.27.02 Downloadable Installation file, S/W Version Date 2020.0701

Comment télécharger

  • If your receiver is connected to the network, download the software update package directly onto the receiver and run the file.
  • Otherwise, download the package onto your PC and transfer the file to the receiver using a USB storage device.
  • Note: Do not run the instrument software executable file on your personal computer. It must be run on the receiver being updated.

Comment installer

Autorisation d'exploitation

Document d'appui

2020-03-31 A.26.10 Downloadable Installation file, S/W Version Date 2020.0220

Comment télécharger

  • If your receiver is connected to the network, download the software update package directly onto the receiver and run the file.
  • Otherwise, download the package onto your PC and transfer the file to the receiver using a USB storage device.
  • Note: Do not run the instrument software executable file on your personal computer. It must be run on the receiver being updated.

Comment installer

Autorisation d'exploitation

Document d'appui

2020-02-07 A.25.08 Downloadable Installation file, S/W Version Date 2020.0207. Latest fully-supported version for instruments running the Windows 7 operating system

Comment télécharger

  • If your receiver is connected to the network, download the software update package directly onto the receiver and run the file.
  • Otherwise, download the package onto your PC and transfer the file to the receiver using a USB storage device.
  • Note: Do not run the instrument software executable file on your personal computer. It must be run on the receiver being updated.

Comment installer

Autorisation d'exploitation

Document d'appui

2019-08-12 A.24.56 Downloadable Installation file, S/W Version Date 2019.0702

Comment télécharger

  • If your receiver is connected to the network, download the software update package directly onto the receiver and run the file.
  • Otherwise, download the package onto your PC and transfer the file to the receiver using a USB storage device.
  • Note: Do not run the instrument software executable file on your personal computer. It must be run on the receiver being updated.

Comment installer

Autorisation d'exploitation

Document d'appui

2015-07-07 A.14.16 Downloadable installation file of the latest software version for instruments running the Windows XP operating system...

Comment télécharger

  • If your receiver is connected to the network, download the software update package directly onto the receiver and run the file.
  • Otherwise, download the package onto your PC and transfer the file to the receiver using a USB storage device.
  • Note: Do not run the instrument software executable file on your personal computer. It must be run on the receiver being updated.

Comment installer

Autorisation d'exploitation

Document d'appui