For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum Version Versionsbeschreibung
2017-02-04 1.2.2.0 See Version Description above.
Veröffentlichungsdatum Version
2017-02-04 1.2.2.0
Version Description
See Version Description above.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0, IviCounter 2.0

Version Description: Updated the implementation of the Counter class’s Pulse width configure method to use the value of channel slope to change the polarity while doing the measurement and updated the implementation of IviCounter.PulseWidth.Configure method to use the Estimate value as provided by the user instead of default value.

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded Installer.

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Supported Instruments

  • 53210A, 53220A, 53230A

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP

Supported Instruments

  • 53210A, 53220A, 53230A

How to Download

  • 1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Run.

How to Install

  • See Readme File

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP

Supported Instruments

  • 53210A, 53220A, 53230A
SHOW MORE