这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

532xx 频率计数器 IVI 仪器驱动程序

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

This driver download installs the IVI-C, IVI-COM, and MATLAB driver components.

Keysight instrument drivers also require that Keysight IO Libraries Suite be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite

Current Version Details
Version 1.0.6.0
Models Supported 53210A, 53220A, 53230A
IO Libraries Required Version 16.0 or greater
IVI Classes Supported IviCounter 1.0 (IVI-COM only)
IviDriver 1.0
Minimum IVI Shared Components Version 2.1.1.0 


 

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0, IviCounter 2.0

Version Description: Updated the implementation of the Counter class’s Pulse width configure method to use the value of channel slope to change the polarity while doing the measurement and updated the implementation of IviCounter.PulseWidth.Configure method to use the Estimate value as provided by the user instead of default value.

发布日期 版本 版本说明
2017-02-04 1.2.2.0 See Version Description above.

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded Installer.

颁发许可证

  • 不要求具有许可证

支持文档