検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

33500シリーズ ファームウェア

33500シリーズ波形発生器の拡張機能と不具合修正を含むファームウェア・アップデートを無料でダウンロードいただけます。33500シリーズ波形発生器のアップデートは、Keysightファームウェア・アップデート・ユーティリティを使用して、測定器のLAN/GPIB/USB IOポートまたはフロント・パネルのUSB「ホスト」ポートから実行できます。

The following improvement has been made in firmware release 5.02:

  • Updated the ACCL version to improve memory leak.
     
リリース バージョン 内容
2019-06-15 5.02 33500 Series Firmware 5.02

ダウンロード方法

  1. Click the Download button.
  2. Save the firmware file to your computer and note the directory where the file is saved. Firmware updates installed over the LAN, GPIB, or USB interface are files with .upd extensions.
  3. Unzip the file to access the .upd file. For updates using a front panel USB drive, the utility extracts the required files from the (unzipped) .upd file.
  4. If not currently installed, download and install the Firmware Update Utility.

インストール方法

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation.
  • If updating from the LAN, USB, or GPIB interface the instrument address is required. With the instrument turned on, pressing Help – About displays the addresses.
  • The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
  • It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

ライセンス

  • ライセンス不要

アドオン・ソフトウェア/ユーティリティ

ダウンロード

インストール:

Instrument

OS

  • Windows 7
  • Windows Vista
  • Windows XP
  • Windows 10

前提条件

  • NOTICE: Downgrading the 335xx Firmware
    Before downgrading to a ‘Previous’ firmware revision, note the firmware revision currently installed (Shift-Help-About).
    Firmware revision 5.02-1.19 and below can be downgraded to any previous (posted) revision.
    Firmware revision 5.02-3.15 and revisions above that can only be downgraded to firmware version 5.02.
     

対象測定器

  • 33509B,33510B,33511B,33512B,33519B,33520B,33521B,33522B,33521A,33522A