您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

335XX / 336XX Function / Arbitrary Waveform Generator IVI and MATLAB Instrument Drivers

For a complete list of all drivers from Keysight, please visit www.keysight.com/find/drivers

發佈日期 版本 版本說明
2017-10-18 2.3.3.0 The driver now sets the impedance to High-Z when the load is set to 0 using Channel.Output.Load property (IviFgen compliant behavior)

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
 

IVI class support: IviDriver 1.0, IviFgen 3.0

 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2017-09-29 2.3.2.0 Fixed an issue with using an arbitrary waveform larger than 65536 points.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
 

IVI class support: IviDriver 1.0, IviFgen 3.0

 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2017-09-01 2.3.1.0 Added support to get arbitrary points and set/get period in existing 33500 models. Added functionality to enable AM DSSC, set pulse hold and get number of points available in volatile memory. Memory leak issue with Ag3352x_CreateArbSequence fixed.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
 

IVI class support: IviDriver 1.0, IviFgen 3.0

 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2017-02-18 2.2.5.0 Fixed issue in the Fgen class related to the underlying SCPI of the Arbitrary.Waveform.set_Frequency and Arbitrary.Waveform.get_Frequency properties.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
 

IVI class support: IviDriver 1.0, IviFgen 3.0

 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2015-10-31 2.2.4.0 Fixed FGEN class defects and an issue with the DownloadFile method.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
 

IVI class support: IviDriver 1.0, IviFgen 3.0
 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.
     

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2015-05-27 2.2.1.0 Minor bug fixes in the IviFgen class

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
 

IVI class support: IviDriver 1.0, IviFgen 3.0

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2015-03-06 2.2.0.0 Updated the help file, added IVI-2014 compliance, rebranded as Keysight Technologies

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
 

IVI class support: IviDriver 1.0, IviFgen 3.0
 

如何下載

  •  
    1. Click the Download button.
    2. Select the appropriate executable file.
    3. Choose Run.
       

如何安裝

  • Run the downloaded installer

授權

  • 不需要授權

支援文件

2014-02-04 2.1.1.0 Added support for 33611A, 33612A, 33621A, 33622A

如何下載

  1. Click the Download button. 
  2. Select the appropriate executable file. 
  3. Choose Download.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2013-04-18 2.0.1.0 Fixes a defect in the 64-bit driver where the ModulePath64 field was empty (64-bit IVI-C Class Compliant calls should now work). No change to the 32-bit driver.

如何下載

  1. Click the Download button. 
  2. Select the appropriate executable file. 
  3. Choose Download.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

下載

安裝於:

PC

作業系統

  • Windows 7
  • Windows Vista
  • Windows XP

必備檔案

  • 無相關資訊

支援的儀器

  • 33521A, 33522A, 33522B, 33521B, 33520B, 33519B, 33512B, 33511B, 33510B, 33509B
2012-08-21 2.0.0.0 IVI, MATLAB Version 2.0.0.0 for 335XX Waveform Generator for 32-bit Windows

如何下載

  • 1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Download.

如何安裝

  • Select run or save to the location of your choice.

授權

  • 不需要授權

支援文件

下載

安裝於:

PC

作業系統

  • Windows 7
  • Windows Vista
  • Windows XP

必備檔案

  • Agilent IO Libraries Suite

支援的儀器

  • 33521A, 33522A, 33522B, 33521B, 33520B, 33519B, 33512B, 33511B, 33510B, 33509B
2010-08-01 1.0.7.0 IVI-COM, IVI-C Version 1.0.7.0 for 3352X for 32-bit Windows

如何下載

  • 1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Run.

如何安裝

  • See Readme File

授權

  • 不需要授權

支援文件