Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

N9020A MXA Signal Analyzer Instrument Software

PLEASE NOTE:

  • Instruments running the Windows 7 and Windows 10 operating system - See the Current Version tab below
  • Instruments running the Windows XP operating system - See the Previous Versions tab below
  • There is no need to recalibrate when new instrument software is installed.

To determine the operating system installed refer to the certificate of authenticity (COA) on the rear panel of the instrument.

Release Date Version Version Description
2019-05-02 A.23.13 Downloadable installation file of the latest software version for instruments running the Windows 7 & 10 operating system.

How to Download

  • If your analyzer is connected to the network, download the software update package directly onto the analyzer and run the file.
  • Otherwise, download the package onto your PC and transfer the file to the analyzer using a USB storage device.
  • Note: Do not run the instrument software executable file on your personal computer. It must be run on the analyzer that is being updated.

How to Install

Licensing

Supporting Documentation