Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

N9000A CXA Signal Analyzer Instrument Software

PLEASE NOTE THE FOLLOWING TWO ITEMS:
   - Instruments running the Windows 7 operating system - See the Current Version tab below
   - Instruments running the Windows XP operating system - See the Previous Versions tab below
To determine the operating system installed refer to the certificate of authenticity (COA) on the rear panel of the instrument

Release Date Version Version Description
2017-09-25 A.19.55 The most current version of the downloadable installation file for instruments with Windows 7 operating system.

How to Download

  • If your analyzer is connected to the network, download the software update package directly onto the analyzer and run the file.
  • Otherwise, download the package onto your PC and transfer the file to the analyzer using a USB storage device.
  • Note: Do not run the instrument software executable file on your personal computer. It must be run on the analyzer that is being updated.

How to Install

Licensing

Supporting Documentation