이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

N9010A EXA Signal Analyzer Instrument Software

PLEASE NOTE:

  • Instruments running the Windows 7 and Windows 10 operating system - See Current Version tab below
  • Instruments running the Windows XP operating sytsem - See Previous Versions tab below
  • There is no need to recalibrate when new instrument software is installed.

To determine the operating system installed refer to the certificate of authenticity (COA) on the rear panel of the instrument.

릴리스 날짜 버젼 버전 설명
2019-08-12 A.24.56 Downloadable installation file of the latest software version for instruments running the Windows 7 and 10 operating system.

다운로드 방법

  • If your analyzer is connected to the network, download the software update package directly onto the analyzer and run the file.
  • Otherwise, download the package onto your PC and transfer the file to the anlayzer using a USB storage device.
  • Note: Do not run the instrument software executable file on your personal computer. It must run on the anlayzer that is being updated.

설치 방법

라이센스

지원 문서