検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

N9010A EXA Signal Analyzer Instrument Software

PLEASE NOTE:

  • Instruments running the Windows 7 and Windows 10 operating system - See Current Version tab below
  • Instruments running the Windows XP operating sytsem - See Previous Versions tab below
  • There is no need to recalibrate when new instrument software is installed.

To determine the operating system installed refer to the certificate of authenticity (COA) on the rear panel of the instrument.

リリース バージョン 内容
2019-08-12 A.24.56 Downloadable installation file of the latest software version for instruments running the Windows 7 and 10 operating system.

ダウンロード方法

  • If your analyzer is connected to the network, download the software update package directly onto the analyzer and run the file.
  • Otherwise, download the package onto your PC and transfer the file to the anlayzer using a USB storage device.
  • Note: Do not run the instrument software executable file on your personal computer. It must run on the anlayzer that is being updated.

インストール方法

ライセンス

説明資料