Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

E5061B Network Analyzers Firmware Update

Please note that you DO NOT need to return your E5061B to Keysight service center for updating the firmware. The E5061B firmware upgrade can easily be performed on your own with the information and tools available on this Web page.

Warning

  • Version B.xx.xx is for the E5061B with Windows 7 only. Use A.xx.xx for the E5061B with Windows XP. Do not install version B.xx.xx on the E5061B with Windows XP. When you install B.xx.xx on E5061B with Windows XP, the firmware will be deleted. Perform System Recovery.
  • Only install this firmware on the E5061B. Attempting to install this Firmware to the E5061A/62A could make them malfunction. If you are the E5061A/62A user, please refer to the download page for the E5061A/62A.
  • Do not attempt to install this firmware on a PC as this may render it unusable.
  • The firmware revision A.01.xx is only for the E5061B-3L5 LF-RF network analyzer. Do not install it to the E5061B RF options.

Other Software Update

Update for a software component of LXI 1.3 installed on E5061B
If your E5061B's HDD C: drive volume label is EL200, KY200, EL203, KY203, or KY204, it is recommended to update a software component of the LXI to the new one. You can get the program for this update by executing the self-extraction file "E5061B_LXI_0.0.24.exe", which is downloadable below.

Notes
• You can check the HDD volume label of your E5061B from its explorer menu.
• The E5061B firmware must be updated to the revision A.02.06 or above before updating this LXI component.

For more details, refer to the PDF document "E5061B LXI 1.3 Component Update Procedure", which is downloadable below.

Update of touch screen driver (only for demo units shipped before October 2009)
The E5061B shipped as demo units in before October 2009 requires updating the touch screen driver, along with updating the firmware to A.01.00 or above. The update procedure and the driver are downloadable below.

Known Issue for B.04.88

  • Auto Orientation might not work correctly on E5061B-3L3
Release Date Version Version Description
2018-06-07 B.05.02 E5061B Firmware Revision B.05.02 (For Windows 7 and Windows 10)

How to Download

  • Click the download button and save the file to a temporary directory on your PC (or instrument).

How to Install

  • 1. Move the E5061B_xx.xx.exe to the instrument.
    2. Press System > Service Menu > Exit to terminate the analyzer application.
    3. Double click E5061B_xx.xx.exe on the instrument.

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

Instrument

Operating System

  • Windows 7
  • Windows 10

Prerequisites

  • Information Not Available

Supported Instruments

  • E5061B