Always update your handheld digital multiemeter with the latest firmware to maximize the performance of the instrument. Please follow all the instructions below step-by-step to ensure the firmware installation is successful.

Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2017-01-19 1.05 Disable DC Filter during measurement at ACmv mode.
Release Date Version
2017-01-19 1.05
Version Description
Disable DC Filter during measurement at ACmv mode.

How to Download

  1. Unzip the zip file to a folder.
  2. Go to folder PL23XX_Prolific_DriverInstaller_v202, click on the PL23XX-M_LogoDriver_Setup_v202.Exe to install the U1173B IR-USB cable driver.

How to Install

  1. Connect the multimeter to your PC via the U1173B IR-USB connectivity cable and turn on the multimeter.
  2. Go to Start > All Programs > Keysight Technologies > Keysight U1281A U1282A Firmware Update > Keysight U1281A U1282A Firmware Update (Version 1.05).
  3. Click

Licensing

  • Does Not Require a License

Installs on: Instrument

Operating System

  • Windows XP SP3
  • Windows 7 SP1
  • Windows Vista SP2
  • Windows 2000 SP4

Prerequisites

  • System Requirements: Intel Pentium 4, 1GHz or equivalent, 512MB RAM, 1GB HDD free space
    Operating Systems: Windows 2000 SP4, Windows XP SP3, Windows Vista SP2, Windows 7 SP1
    Required accessory: U1173B IR-USB Connectivity Cable

Supported Instruments

  • U1281A, U1282A

How to Download

  1. Unzip the zip file to a folder.
  2. Go to folder PL2303_XPVistaWin7_Driver, click on the PL2303_XPVistaWin7Driver. Exe to install the U1173B IR-USB cable driver.
  3. Double click the Setup.exe file to install the program.

How to Install

  1. Connect the multimeter to your PC via the U1173B IR-USB connectivity cable and turn on the multimeter.
  2. Go to Start > All Programs > Keysight Technologies > Keysight U1281A U1282A Firmware Update > Keysight U1281A U1282A Firmware Update (Version 1.04).
  3. Click "Auto Search COM Port" button to search and detect the unit. The model number, serial number and current firmware version of the multimeter will be displayed in the "Model Number", "Serial Number" and "Current Version" field.
  4. Make sure the instrument is in connected status before you start firmware update. Click "Upload Firmware" to start firmware update.
  5. The multimeter will reset and recover itself after the firmware update.

Licensing

  • Does Not Require a License

Installs on: Instrument

Operating System

  • Windows XP SP3
  • Windows 7 SP1
  • Windows Vista SP2
  • Windows 2000 SP4

Prerequisites

  • System Requirements: Intel Pentium 4, 1GHz or equivalent, 512MB RAM, 1GB HDD free space
    Operating Systems: Windows 2000 SP4, Windows XP SP3, Windows Vista SP2, Windows 7 SP1
    Required accessory: U1173B IR-USB Connectivity Cable

Supported Instruments

  • U1281A, U1282A

How to Download

  1. Unzip the zip file to a folder.
  2. Go to folder PL2303_XPVistaWin7_Driver, click on the PL2303_XPVistaWin7Driver. Exe to install the U1173B IR-USB cable driver.
  3. Double click the Setup.exe file to install the program.

How to Install

  • 1. Connect the multimeter to your PC via the U1173B IR-USB connectivity cable and turn on the multimeter.
    2. Go to Start > All Programs > Keysight Technologies > Keysight U1281A U1282A Firmware Update > Agilent U1281A U1282A Firmware Update (Version 1.03).
    3. Click “Auto Search COM Port” button to search and detect the unit. The model number, serial number and current firmware version of the multimeter will be displayed in the “Model Number”, "Serial Number" and "Current Version" field.
    5. Make sure the instrument is in connected status before you start firmware update. Click “Upload Firmware” to start firmware update.
    6. The multimeter will reset and recover itself after the firmware update.

Licensing

  • Does Not Require a License

Installs on: Instrument

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP
  • Windows 2000

Prerequisites

  • Prerequisite:
    System Requirements: Intel Pentium 4, 1GHz or equivalent, 512MB RAM, 1GB HDD free space
    Required accessory: U1173B IR-USB Connectivity Cable

Supported Instruments

  • U1281A, U1282A
SHOW MORE