这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

E36xx 直流电源 IVI 仪器驱动程序

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

This driver download installs the IVI-C, and IVI-COM driver components.

Keysight IVI drivers also require the Keysight IO Libraries Suite to be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite

Current Version Details
Version 1.1.6.0
Models Supported E3632A, E3633A, E3634A, E3640A, E3641A, E3642A, E3643A, E3644A, E3631A, E3645A, E3646A, E3647A, E3648A, E3649A
IO Libraries Required Version 15.0 or greater
Driver Types IVI-C (32-bit)*
IVI-COM (32-bit)*
IVI Classes Supported IviDCPwr 2.0
IviDriver 1.0
Minimum IVI Shared Component Version 1.5.0.0 
OS Support 2000, XP, Vista*, 7*

*This driver can be installed on Windows Vista 64-bit and Windows 7 64-bit, but can only be accessed by 32-bit applications (this is called WoW64 ).
 

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviDCPwr 3.0

发布日期 版本 版本说明
2019-04-30 1.5.0.0 Added SCPIs and model support of E36231A, E36232A, E36233A and E36234A.

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 8
  • Windows 7
  • Windows 10

前提条件

支持的仪器

  • E3649A, E3648A, E3647A, E3646A, E3645A, E3644A, E3643A, E3642A, E3641A, E3640A, E3634A, E3633A, E3632A, E3631A, E36102A, E36102B, E36103A, E36103B, E36104A, E36104B, E36015A, E36105B, E36106A, E36106B, E36311A, E36312A, E36313A, E36231A, E36232A, E36233A, E36234A

相关链接