What are you looking for?
U-Series USB Average Sensor Upgrade Utility
Click on the url and unzip the zip file contents onto a local directory. This zip file contains the executable file and help file for installing the Utility in order to upgrade the U-Series USB Average Sensors.
If you are unable to view help files downloaded from the Keysight website:
In September 2005, Microsoft® released a security patch for Windows® operating systems that protects PCs from the threat of malicious code that could reside in compiled HTML help files (*.chm files). When a *.chm file is downloaded to a PC that has the patch installed, the file opens with one of the following error messages displayed:
- Action Canceled
- The page cannot be displayed
Workaround: After downloading the file to your PC, open it from the location it was saved and a security warning appears. To view the help system, clear the checkmark from the "Always ask before opening this file" check box. The help system can now be viewed from the PC. Alternatively, right-click the file you want to open, click Properties and then click Unblock.
Note: No workaround exists for viewing *.chm files remotely. You must first download the file to your PC and then use the workaround described above.
Microsoft is a U.S. registered trademark of Microsoft Corporation.
Windows and MS Windows are U.S. registered trademarks of Microsoft Corporation.
發佈日期 | 版本 | 版本說明 |
---|---|---|
2013-01-21 | R01.07.00 | The U-Series USB Average Sensor Upgrade Utility. |
發佈日期 | 版本 |
---|---|
2013-01-21 | R01.07.00 |
Version Description |
---|
The U-Series USB Average Sensor Upgrade Utility. |
如何下載
Click on the url and unzip the zip file contents onto a local directory. This zip file contains the executable file and help file for installing the Utility in order to upgrade the U-Series USB Average Power Sensors.
如何安裝
授權
- Does Not Require a License
Installs on: PC
作業系統
- Windows 8
- Windows 7
- Windows Vista
- Windows XP SP3
- Windows XP SP2
參加條件
Windows® XP Professional (Service Pack 2 or higher) - Agilent IO Libraries 16.0 or higher
Windows Vista Business - Agilent IO Libraries 16.0 or higher
Window 7 - Agilent IO Libraries 16.0 or higher
Window 8 - Agilent IO Libraries 16.3 or higher
支援的儀器
- U2000A,U2001A,U2002A,U2004A,U2000B,U2000HU2001B,U2001H,U2002H,U8485A,U8481A