What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
34410A DMM Firmware
キーサイトは、最新のバグ修正とセキュリティパッチを含む、利用可能な最新バージョンを使用することをお勧めします。
リリース | バージョン | 内容 |
---|---|---|
2017-02-08 | 2.43 | 34410A Firmware Update Revision 2.43 |
リリース | バージョン |
---|---|
2017-02-08 | 2.43 |
Version Description |
---|
34410A Firmware Update Revision 2.43 |
ダウンロード方法
- Download and install the 34410A Firmware Update Utility located in the "Add-On Software/Utilities" section at the bottom of this page. If you already have the Firmware Update Utility installed on your computer, skip this step.
- Use the Download button to download the Keysight 34410A Firmware.
- Unzip the Keysight 34410A Firmware file, making note of where you store the unzipped file.
- Open the Firmware Update Utility (Start -> Programs -> Keysight -> Firmware Update Utility).
- Click Next.
インストール方法
- Click Browse and locate the firmware update file that you unzipped. Highlight the file and select Open.
- Click Next.
- Select the I/O interface (GPIB, LAN, or USB) that connects your DMM to your PC.
- Choose the settings necessary for communication (GPIB address, IP address, USB ID).
- Click Update. NOTE: This update will take several minutes and the DMM will display status messages and automatically reboot when completed. DO NOT cycle or interrupt power to the DMM during the update process.
- After this is completed, exit the update utility.
- Refer to the DMM front panel and note if there are any errors (the ERROR light will be on in the display).
- The update process is now complete.
Note: There is no need to re-calibrate the DMM when this new firmware is installed.
ライセンス
- Does Not Require a License
説明資料
ダウンロード方法
- Download and install the 34410A Firmware Update Utility located in the "Add-On Software/Utilities" section at the bottom of this page. If you already have the Firmware Update Utility installed on your computer, skip this step.
- Use the Download button to download the Keysight 34410A Firmware.
- Unzip the Keysight 34410A Firmware file, making note of where you store the unzipped file.
- Open the Firmware Update Utility (Start -> Programs -> Keysight -> Firmware Update Utility).
-
Click Next.
インストール方法
- Click Browse and locate the firmware update file that you unzipped. Highlight the file and select Open.
- Click Next.
- Select the I/O interface (GPIB, LAN, or USB) that connects your DMM to your PC.
- Choose the settings necessary for communication (GPIB address, IP address, USB ID).
- Click Update. NOTE: This update will take several minutes and the DMM will display status messages and automatically reboot when completed. DO NOT cycle or interrupt power to the DMM during the update process.
- After this is completed, exit the update utility.
- Refer to the DMM front panel and note if there are any errors (the ERROR light will be on in the display).
- The update process is now complete.
Note: There is no need to re-calibrate the DMM when this new firmware is installed.
ライセンス
- Does Not Require a License
説明資料
アドオン・ソフトウェア/ユーティリティ
SHOW MORE