検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

82351A Installation Driver (Only required for IO Libraries 14.2 or below)

The 82351A is the latest half-height 3.3V PCIe™-GPIB interface card that is highly integrated to the next generation of smaller form factor PCIe™-based PC or workstations.

Before installing the driver, please ensure your PC meets the minimum system requirements with Microsoft® Windows® 2000/XP Professional and latest version of Keysight IO Libraries Suite 14.2 installed.

To obtain the driver for 82351A, click on the link and save the file to any location on your hard disk. Double-click on the 82351A_setup.exe file to run the installer. Follow the instructions on the screen to install the driver. Once the driver installation has completed, your 82351A will be working successfully!

Microsoft and Windows are U.S. registered trademarks of Microsoft Corporation.
PCIe and PCI EXPRESS are trademarks or registered trademarks of PCI-SIG.

過去のバージョンはありません