What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
E1852B Software/Firmware Download
The installation procedure is in three parts:
Part 1: Uninstall any previous E1852B software
Part 2: Installs the MMI to the PC
Part 3: Installs the Firmware to the E1852B
Note: Contains version B.00.07 MMI, DLL, and Firmware for use with Keysight E1852B only
Part 1: Uninstall
Note: This must be carried out if the host PC has previously installed E1852B software
If the host PC has had E1852B software previously installed. Select [Start], [Settings], [Control Panel], [Add/Remove Programs]
Select E1852B and press the [Add/Remove...] key. Follow the on screen instructions to uninstall
Note: If and when prompted delete all files including *.dll files
Part 2: MMI and DLL Installation
- If your PC does not have the winzip application. Download and Install winzip from the link at www.winzip.com
- Download the software to your host PC from the Download link, recommended directory C:\WINDOWS\TEMP\E1852B
- Double click on the zipped file named 'E1852B-B0007.zip'. Select [Extract], [Save]. Recommended directory C:\WINDOWSTEMPE1852B
- Open the folder C:\WINDOWSTEMPE1852B. Double click the file named 'setup.exe' and follow the on screen instructions to install the MMI and DLL to your host PC
Part 3: Firmware Installation
- Connect the E1852B to the PC with the parallel cable provided
- On the PC select [Start], [Programs], [Keysight Technologies] and click the E1852B Debug version. Note: only the Debug version will download FW to the E1852B.
- From the E1852B System menu select the host PC's serial port (default Com1) from the Firmware Update section and press Download
- Highlight the file *.bsf file and select [Open]
- The procedure will then prompt for the following; 1. Connect the serial cable provided from the PC's serial port and the E1852B serial port; 2. Recycle the power, Switch the E1852B [Off] then [On] before clicking [OK]
- Both the Firmware Version & PC DLL Version within the E1852B System menu, Software Version section should now be the same, example B.00.07.
- Close the E1852B software and reopen. On the PC select [Start], [Programs], [Keysight Technologies] and click either the standard or debug mode version.
A Keysight recomenda usar a versão mais atual, que inclui as correções de bugs e arquivos de segurança mais atualizados disponíveis.
Data de lançamento | Versão | Descrição da Versão |
---|---|---|
2003-04-01 | B.00.07 | MMI (PC User Interface) software and firmware files. |
Data de lançamento | Versão |
---|---|
2003-04-01 | B.00.07 |
Version Description |
---|
MMI (PC User Interface) software and firmware files. |
Como Baixar
See Above
Como Instalar
See Above
Licenciamento
- Does Not Require a License
Documentação de suporte
Não há versão de software disponível
SHOW MORE