The B.01.31 Phase Noise Measurement Utility can be obtained using one of the following two methods:

  • If you already have a license for this personality you can download the latest version from this site for free to a Microsoft Windows based Personal Computer.
  • If you do not have a license for this personality you will need to order an E440xBU-226 upgrade kit.

Note: This Phase Noise Measurement Utility version is only for use with ESA-E Series Spectrum Analyzers with Option B72 (expanded memory). If you do not have Option B72 the latest version that can be installed is A.01.15 available below. only for use with ESA-E Series Spectrum Analyzers with firmware version A.07.03 or newer.

The "ESA Personality Installation Procedure" will guide you through:

  • Downloading the installation image
  • Creating an installation floppy disk set
  • Loading the software into your ESA
  • Verifying the installation
Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2003-04-19 B.01.31 Downloadable installation file.
Release Date Version
2003-04-19 B.01.31
Version Description
Downloadable installation file.

How to Download

  • See the Installation Procedure

Licensing

  • Requires a License

Installs on: PC / Instrument

Prerequisites

  • See the Installation Procedure

Supported Instruments

  • E440xBU-226

How to Download

  • See the Installation Procedure

Licensing

  • Requires a License

Installs on: PC / Instrument

Prerequisites

  • See the Installation Procedure

Supported Instruments

  • E440xBU-226
SHOW MORE