您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

E6432A Microwave Synthesizer: VXI Plug&Play Universal Instrument Driver

The E6432A VXI plug&play driver requires the following hardware and software:

  • Windows NT 4.0®1 Framework
  • Windows NT 4.0 computer with Service Pack 3 or higher
  • Minimum of 32 MB of RAM or higher
  • CD-ROM drive
  • Keysight E8403A C-size VXI mainframe or equivalent

One of the following Slot 0 Modules:

  • E8491A IEEE-1394 PC Link to VXI Using a PCI to IEEE-1394 Interface (FireWire)
  • E2094G I/O library version G.02.02 (which contains VISA®2 1.1) or higher
  • E623x Embedded VXI Pentium PC Controller or equivalent
  • E2094G I/O library version G.02.02 (which contains VISA®2 1.1) or higher
  • NI VXI-MXI-2 - Using a PCI-MXI-2 Interface
  • National Instrument® VISA?2 I/O library version 2.0 or higher
  • E6432A driver revision A.01.00 or higher
  • National Instruments CVI run-time engine, Revision 5.5, is needed by the E6432A driver's soft front panel; this must be installed prior to running e6432a_plugandplay_driver.exe. Refer to National Instruments for a CVI run-time engine. 

1Windows NT 4.0 is a registered trademark of Microsoft Corporation.

2VISA is a registered trademark of National Instruments Corporation.

發佈日期 版本 版本說明
2002-10-25 n/a e6432_plug&play_driver.exe

如何下載

  • See Above

如何安裝

  • See Above

授權

  • 不需要授權
下載

安裝於:

PC

作業系統

  • Windows NT

必備檔案

  • See Above

支援的儀器

  • E6432A