Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

Downloadable Vector Network Analyzer Uncertainty Calculator

Read the license agreement before downloading the Uncertainty Calculator program.
To do so, scroll down to Supporting Documentation and click License Agreement. By downloading this Uncertainty Calculator program, you agree to be bound by the terms of this license agreement. If you do not agree to all of these terms, do not download the program.

Date de mise en circulation Version Description de la version
2018-11-07 A.5.0.8.0 The Uncertainty Calculator helps you determine measurement uncertainty due to your vector network analyzer and calibration kit.

Comment télécharger

  • 1. Click the Download button and download to your computer either 32 bit or 64 bit installer. If you have a 32 bit operating system install the 32 bit version. Otherwise, install the 64 bit version. Note, the 64 bit installer will install the files needed for both the 32 bit and 64 bit office versions in the location where the spreadsheet will look for.

Comment installer

  • 1. After you click the download button you will have the option to Run or Save. Select Run.
    2. Both the 64 bit and 32 bit installers place Readme.txt, Change Log.txt, and VNAUncert.dll in C:\Program Files\Keysight\VNA Uncertainty. The 64 bit installer also places VNAUncert64.dll in the same directory.
    3. The installer places KeysightUncert.xlsm in C:\Users\Public\Documents\Keysight. This is the spreadsheet to be opened with Excel.
    4. After opening the spreadsheet in Excel, select the [Select Network Analyzer] button.
    5. Follow the instructions provided in the program to display measurement uncertainty data.

Autorisation d'exploitation

  • Ne requiert aucune licence

Document d'appui

Téléchargez

S'installe sur:

PC

Système d'exploitation

  • Windows 10

Préalables

  • Information non-disponible