您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

可下載的向量網路分析儀量測不確定性計算軟體

下載不確定性計算軟體之前,請先閱讀授權合約。
請往下捲動到「支援文件」標籤並且點選授權合約。一旦下載此不確定性計算軟體,代表您同意此授權合約所列條款的規範。如不同意任何的條款,請勿下載本軟體。

發佈日期 版本 版本說明
2018-11-07 A.5.0.8.0 The Uncertainty Calculator helps you determine measurement uncertainty due to your vector network analyzer and calibration kit.

如何下載

  • 1. Click the Download button and download to your computer either 32 bit or 64 bit installer. If you have a 32 bit operating system install the 32 bit version. Otherwise, install the 64 bit version. Note, the 64 bit installer will install the files needed for both the 32 bit and 64 bit office versions in the location where the spreadsheet will look for.

如何安裝

  • 1. After you click the download button you will have the option to Run or Save. Select Run.
    2. Both the 64 bit and 32 bit installers place Readme.txt, Change Log.txt, and VNAUncert.dll in C:\Program Files\Keysight\VNA Uncertainty. The 64 bit installer also places VNAUncert64.dll in the same directory.
    3. The installer places KeysightUncert.xlsm in C:\Users\Public\Documents\Keysight. This is the spreadsheet to be opened with Excel.
    4. After opening the spreadsheet in Excel, select the [Select Network Analyzer] button.
    5. Follow the instructions provided in the program to display measurement uncertainty data.

授權

  • 不需要授權

支援文件