The hardware security key provided with the original shipment must be the only key installed on LPT1 parallel port during the update process. If you do not have a hardware security key, contact your local sales office to purchase one.

Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum Version Versionsbeschreibung
2004-02-20 A.02.00 Version A.02.00 provides an update from revision A.01.00 to revision A.02.00. This update allows Microsoft Word 97 to work with the auto report feature in the Report Generator software. This fixes problems that occur when using the European numbering
Veröffentlichungsdatum Version
2004-02-20 A.02.00
Version Description
Version A.02.00 provides an update from revision A.01.00 to revision A.02.00. This update allows Microsoft Word 97 to work with the auto report feature in the Report Generator software. This fixes problems that occur when using the European numbering

How to Download

  • Select the executable file. Choose Run.

How to Install

  • Choose Run.

Lizenzierung

  • Does Not Require a License

Installs on: PC

Voraussetzungen

  • See Above

Supported Instruments

  • 85878A
Keine Softwareversion verfügbar
SHOW MORE