Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

85878A Report Generator Software

The hardware security key provided with the original shipment must be the only key installed on LPT1 parallel port during the update process. If you do not have a hardware security key, contact your local sales office to purchase one.

Date de mise en circulation Version Description de la version
2004-02-20 A.02.00 Version A.02.00 provides an update from revision A.01.00 to revision A.02.00. This update allows Microsoft Word 97 to work with the auto report feature in the Report Generator software. This fixes problems that occur when using the European numbering

Comment télécharger

  • Select the executable file. Choose Run.

Comment installer

  • Choose Run.

Autorisation d'exploitation

  • Ne requiert aucune licence