Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

PathWave Model Builder (MBP) Software

Choose a platform:
Release Date Version Version Description
2020-04-23 2020 Update 1.0 PathWave Model Builder 2020 Update 1.0 adds the support for AgeMOS simulation and model tuning by invoking native Spectre.

Note: The minimum license version required to run this software is 2019.02. If you are a supported customer and your date-based license version is less than 2019.02, please contact the Keysight EDA Business Support Center for an updated license file. If you are supported and have a numeric license version (i.e. 3.2), login to the Keysight Software Manager to obtain your updated licenses before installation. For other licensing tasks, see "How to Obtain a License".

2020-01-22 2020 PathWave Model Builder (MBP) 2020 adds the new UTSOI2 model extraction package, the new MOSRA-API based model extraction package, the new Lib Tweaking feature and the enhancements in Corner Tweaking.

Note: The minimum license version required to run this software is 2019.02. If you are a supported customer and your date-based license version is less than 2019.02, please contact the Keysight EDA Business Support Center for an updated license file. If you are supported and have a numeric license version (i.e. 3.2), login to the Keysight Software Manager to obtain your updated licenses before installation. For other licensing tasks, see "How to Obtain a License".

2019-02-07 2019 MBP 2019 adds the new MOSRA level 3 HCI and BTI model extraction package, the new re-centering module, the support of the latest BSIM-BULK version, and the enhancements in the corner tweaking module.

Note: The minimum license version required to run this software is 2018.04. If you are a supported customer and your date-based license version is less than 2018.04, please contact the Keysight EDA Business Support Center for an updated license file. If you are supported and have a numeric license version (i.e. 3.2), login to the Keysight Software Manager to obtain your updated licenses before installation. For other licensing tasks, see "How to Obtain a License".

How to Download

How to Install

Licensing

Supporting Documentation

Hotfixes / Software Patches

2017-04-28 2017 MBP 2017 includes the new SRAM cell model generation package, enhanced model extraction flows for statistical model and compact models, updated script API, improved UI, and the support for the latest model versions.

Note: The minimum license version required to run this software is 2017.01. If you need to upgrade your license, see "How to Obtain a License".

How to Download

How to Install

Licensing

Supporting Documentation

Hotfixes / Software Patches

2016-02-09 2016.01 MBP 2016.01 includes the new corner tweaking module, improvements in statistical modeling, enhanced extraction flow for BSIM-IMG, support of UTSOI and other new model versions, and the 64-bit OS support.

Note: The minimum license version required to run this software is 3.2. If you need to upgrade your license, see "How to Obtain a License".

How to Download

How to Install

Licensing

Supporting Documentation

Hotfixes / Software Patches

2014-06-26 2014.04 MBP 2014.04 supports integrated data flow on our device modeling platform, BSIM-CMG and BSIM6 extraction flows, new model versions, and improvements in statistical modeling.

Note: MBP 2014.04 does not require new licenses if you are currently on MBP 2013.01. New licenses are required if you are using any prior Accelicon MBP version. If you need to upgrade your license, see "How to Obtain a License".

2013-03-12 2013.01 MBP 2013.01 supports integrated data flow on Keysight device modeling platform, modeling SOP, circuit-based model extraction, built-in PCA analysis for variation modeling, and a GUI-based custom model extraction environment.

Note: MBP 2013.01 does not require new licenses if you are currently on MBP 2012.07. New licenses are required if you are using any prior Accelicon MBP version. If you need to upgrade your license, see "How to Obtain a License".

2012-08-17 2012.07 Model Builder Program (MBP) 2012.07 for Windows.

Note: MBP 2012.07 requires new 3.0 version licenses. The licenses will not be backward compatible with prior Accelicon MBP/MQA releases as these releases use a different vendor daemon.

Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows XP

Prerequisites

Related Links

2012-01-04 2011.2.0 Requires FlexNet 11 Licensing Software
Download

Installs on:

PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP

Prerequisites

Supported Instruments

  • Not Applicable

Related Links