Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

B4622A DDR2/3 Protocol Compliance and Analysis Tool

When purchased with a logic analyzer, the application software you order is installed on the instrument hard drive. If you are controlling a logic analyzer from a host PC, you must install the following software before you can make measurements.

If you are controlling a logic analyzer from a host PC, you must install the following software before you can make measurements.

To use this software, you must install the latest version of three packages:

  • Logic and Protocol Analyzer Software
  • B4621A DDR2 and DDR3 Bus Decoder
  • and this software

After you have downloaded the software, double-click on the setup file then follow the instructions which are displayed.

Release Date Version Version Description
2015-02-09 05.90 For installing the compatible DDR2/3 protocol compliance and analysis tool software package.

How to Download

  • Click the download button, select file and save.

How to Install

Licensing

  • Requires a License

Supporting Documentation

Add-On Software / Utilities

Download

Installs on:

PC / Instrument

Operating System

  • Windows 8
  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows Server 2003 SP2
  • Windows Server 2008 SP2
  • Windows Server 2008 R2 SP1
  • Windows 8.1

Prerequisites

Supported Instruments

  • 16900 series and U4154A Logic Analyzers

Related Links