Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

N9330A Handheld Cable and Antenna Tester Firmware

Release Date Version Version Description
2008-10-22 A.01.65 Firmware file available for download...

How to Download

  1. Click the Download button
  2. Save file to your PC

How to Install

  1. Extract and copy N9330A.bin file to the ROOT directory of USB memory stick.
  2. Insert this USB stick to the USB port on the top panel of N9330A.
  3. Press {SYS} > {Upgrade} to upgrade the firmware.
  4. Cycle the power to N9330A when notice "Upgrade Complete. Effective after Restart."
    Notice: When upgrading the N9330A firmware from an older version, unrecognized fonts will be displayed instead of this message. Please restart N9330A as well.
  5. Repeat the step 4 and 5. When unit is powered on, press {SYS} > {More} > {Status} to check the firmware version. It should be A.01.65.
    Notice: If the display is black when N9330A is powered on, please adjust the "Contrast", by pressing {Contrast}, and then turn the knob, to see the displayed information.

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

Instrument

Prerequisites

  • None

Supported Instruments

  • N9330A