Click on the .exe files and save it to a directory on your system. Then, from that directory, unzip it and run the setup.exe file. To install follow the prompted on-screen install directions.

Windows is a U.S. registered trademark of Microsoft Corporation.

Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2008-01-31 v2.00.0 Save the file to the suggested folder and run setup.exe from that location.
Release Date Version
2008-01-31 v2.00.0
Version Description
Save the file to the suggested folder and run setup.exe from that location.

How to Download

  • Information Not Available

How to Install

  • See Readme File

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows XP
  • Windows 2000

Prerequisites

  • Not Applicable

Supported Instruments

  • See Above
No previous versions available
SHOW MORE