Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

KTCC Installer (Trial version 3.8.7.73)

The Keysight Test Coverage Consultant (KTCC) is a Windows PC standalone application installable on to a notebook PC enabling the user to conveniently create test coverage reports on the go.

Keysight Test Coverage Consultant, powered by Aster Technologies’ Testway engine, will objectively review the board CAD files or board test files to generate a comprehensive report using the PCOLA-SOQ metrics.

The software has the intelligence to analyze circuits with Keysight’s In-Circuit test technologies to determine the types of tests available to each component. The user selects the test technologies licensed on the target Keysight In-Circuit test system and the tool will produce the test coverage report using the licensed test features. Selecting or de-selecting the Keysight’s In-Circuit test technologies will alter the test coverage accordingly.
 

Дата выпуска Версия Описание версии
2016-03-30 3.8.7.73 Trial version does not require license

Как загрузить

  • Click

Как установить

  • 1. Double click on the installer (.exe).
    2. If the User Account Control dialog box appears, click Yes to allow the installation to continue.
    3. Follow the instructions on the screen to complete the installation.

Лицензии

  • Лицензия не требуется
Загрузить

Устанавливается на:

PC

Операционная система

  • Windows 7
  • Windows Vista
  • Windows XP

Предварительные условия

  • Информация недоступна

Поддерживаемые приборы

  • KTCC software